Airport Vertical Samples¶
Create a new airport¶
- Find
POST /airports
. Change all the details in Notepad as per the example below:
{ "name": "Amsterdam Schiphol Airport", "iata-code": "AMS", "icao-code": "EHAM", "country": "NL", "time-zone": "CET", "geo-coordinate": { "latitude": 52.308056, "longitude": 4.764167 } }
After changing the data structure to your needs, you can insert the data.
Run the
POST
call.- If
POST
is successfully executed, the response code will be200
. The airport is now created and stored in Aviation Data Hub and accessible at any time.
Query the created airport¶
For more information regarding filtering, please refer to the ADH User Manual.
- Go to
GET /airports/{iata-code}
and prepare it with the parameter set toAMS
. - Execute the
GET
request and check the server response. - If the execution is successful, you will see the response code 200 and the airport details under the response body.
Adding additional attributes¶
- You can add additional attributes or information by using the previously edited value in Notepad. The additional attributes need to be added in a valid JSON format.
Add the attribute "terminal" in Notepad, as per the example below:
{ "name": "Amsterdam Schiphol Airport", "iata-code": "AMS", "icao-code": "EHAM", "country": "NL", "time-zone": "CET", "geo-coordinate": { "latitude": 52.308056, "longitude": 4.764167 }, "terminal": 3 }
Run the
POST
call.- When the
POST
request is successfully executed, the response code will be200
. The airport is now updated. - Repeat the steps in Exercise 2 above, and your added attribute will be shown.
Community
Connect and Collaborate with Industrial Professionals and Join the Community!Click to load comments