Changelog¶
The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.
[1.1.2] - 2026-09-16¶
Added¶
- Added support for the
go-buddycommand in the specification.
[1.1.1] - 2026-07-16¶
Added¶
- US Deployment support (us-east-1).
[1.1.0] - 2026-04-28¶
IMPORTANT CHANGES¶
- API Endpoint Update: New domain and API path for the Structure API.
- Old Endpoint:
https://api.bpcloud.siemens.com/structure/* - New Endpoint:
https://eu.buildingx.siemens.com/api/openness/structure/* - Action Required: Please update your integrations to use the new endpoint.
- Grace Period: The old domain will remain available until 31 March 2027, after which it will be permanently retired.
- Old Endpoint:
[1.0.35] - 2025-09-12¶
- Enrich Point with additional attributes: unit, enum, systemAttributes
[1.0.34] - 2025-02-04¶
- Fixed maestro version in order to realign to 1.0.31
- Fixed vulnerabilities
[1.0.33] - 2024-11-12¶
Updated¶
- Updated changelog
[1.0.32] - 2024-11-12¶
Updated¶
- Aligned the documentation and corrected spelling errors
[1.0.30] - 2024-06-18¶
Updated¶
- Fix minor issue with schema from 'Create Equipment' and 'Update Equipment'
[1.0.28] - 2024-03-12¶
Updated¶
- Updating spec from
Structure API->Building Structure API.
[1.0.25] - 2023-09-29¶
Updated¶
- Fixes to specification to reflect that client generated IDs are not supported when creating Point and Equipment.
[1.0.24] - 2023-06-06¶
Added¶
- 'Create Point' operation. Creation of points is exposed for evaluation purposes until the new subscription is released by September 2023.
[1.0.23] - 2023-05-25¶
Updated¶
- Fix typo of "writeable"
- Fix inconsistency, "/has-points" should take an array as primary data
[1.0.22] - 2023-05-15¶
Added¶
- Point.source property
[1.0.16] - 2022-12-15¶
Added¶
- Equipment, PointGroups endpoints to enable management of building equipment topology
[1.0.1] - 2022-09-28¶
Updated¶
- Location ID schema
[1.0.0] - 2022-09-27¶
Added¶
- Structure API released