The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

RESTful API for reading fire events of your site.

Changelog

The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.

[1.1.0] - 2026-06-17

Added

  • Support for hardware tree based response in the configuration API.

[1.1.0-rc1] - 2026-05-18

IMPORTANT CHANGES

  • API Endpoint Update: New domain and API path for the Fire API.
    • Old Endpoint: https://api.bpcloud.siemens.com/fire/*
    • New Endpoint: https://eu.buildingx.siemens.com/api/openness/fire/*
    • Action Required: Please update your integrations to use the new endpoint.
    • Grace Period: The old domain will remain available until 31 March 2027, after which it will be permanently retired.

[1.0.3] - 2025-10-06

Removed

  • Commands API endpoint

[1.0.2] - 2025-07-31

Updated

  • Enforce commanding for geofence enabled

[1.0.1] - 2025-06-06

  • Enable location API
  • Add new points API

[1.0.0] - 2025-05-27

Fix

  • deprecate locations API

[0.0.20] - 2025-05-15

Updated

  • Update response body of Configuration API

[0.0.19] - 2025-03-12

Added

  • Site Information and Channels API, supports retrieving channels data along with its dynamic data

[0.0.18] - 2024-11-05

Added

  • New Commands API

[0.0.16] - 2024-11-05

  • Added linting

[0.0.15] - 2024-11-05

  • Added Parent CustomerText Level 1, 2, 3 Attributes for the events API

[0.0.14] - 2024-09-25

  • revert deprecate locations API

[0.0.13] - 2024-09-24

  • Added fire.api-manager.openapi.yaml to the package in the dist subfolder

[0.0.12] - 2024-09-23

  • Enhance Fire API offering for events by adding event source as response

[0.0.11] - 2024-08-08

  • Aligned the documentation and corrected spelling errors

[0.0.10] - 2023-05-28

  • deprecate locations API

[0.0.7] - 2023-09-28

Updated

  • added panel device example for the /device API

[0.0.6] - 2023-07-21

Updated

  • remove page[limit] query parameter for the /device API

[0.0.5] - 2023-07-15

Updated

  • Update Base url path of fire API for the developer portal

[0.0.3] - 2023-06-27

Updated

  • Update env configuration for Fire APIs

[0.0.1] - 2023-05-26

Added

  • First version of 'Fire API'