The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

RESTful API for creating and managing various objects in the Lifecycle Twin.

Create folder

Endpoint - /documents

HTTP Method – POST

Request

Headers

ParameterDescription
clientname(mandatory) Portfolio name
authorization(mandatory) Authentication token
projectId(mandatory) Project identifier

Body

JSON of the folder definition

Media type : application/json

Example:

{
    "Name": "DWG Drawings",
    "Parent": {
        "Id": "723d3996-6b6d-4429-93bc-0d9bb4472e31"
    },
    "IsFolder":  **true**
}

Note

  • Parent Id is mandatory and must be the ID of a folder. Without it, the folder is created but does not appear in the user interface.
  • IsFolder: true is mandatory to create a folder.

Response

HTTP status code 200

Body

The response body contains the ID of the created folder.

Media type: application/json

Example:

{
    "Value": "9c2e4b64-ab91-470b-92ff-62d78263478e"
}