The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Point Value Ingest API Share llms optimized content

RESTful API for setting values of a Point.

Quick Start

Getting started with using add Point Value Ingest API involves the following steps:

  1. Create an account and a machine user.
  2. Create a JSON Web Token (JWT) by using the machine user credentials.
  3. Make API requests using the JWT.

Note

In the following examples we are:

1. making use of a Linux/MacOS shell in which environmental variables are
   set using the `export` command. In other environments it may be different,
   e.g. Windows uses the `set` command instead.

2. using the `curl` as a client. But the API can be used in any programming
   language with an HTTP Client, e.g. Go, Python, NodeJS, Javascript and Java.

Create an account and a machine user

The Getting Started page documents the required steps to get a hold of the clientId, clientSecret and partitionId.

Create a token

Use the values described in the Authorization section to construct the Create Token request.

Example request

export CLIENT_ID=<YOUR_CLIENT_ID>
export CLIENT_SECRET=<YOUR_CLIENT_SECRET>

curl https://eu.buildingx.siemens.com/oauth/token \
  -H 'content-type: application/json' \
  -d "{
            \"client_id\":\"$CLIENT_ID\",
            \"client_secret\":\"$CLIENT_SECRET\",
            \"audience\":\"https://horizon.siemens.com\",
            \"grant_type\":\"client_credentials\"
      }"

To run this example yourself, set the CLIENT_ID and CLIENT_SECRET first.

Example response

{
  "access_token": "eyJ0eXAiOiUSJ9.eyJpc3MiOiJdGlhbHMifQ.MJpcxLfyOt",
  "token_type": "Bearer",
  "expires_in": 86400
}

The token, or JWT (JSON Web Token), is the value of the access_token property in the response.You can now use it by passing it in the Authorization header of any subsequent API requests.The expires_in property represents the number of seconds your token is valid, usually, the value corresponds to 24 hours. When this time has elapsed you will need to create a new token.

Now you have all you need to start using the API. As a last step of preparation set the token and partitionId as environmental variables.

export PARTITION=<YOUR_PARTITION_ID>
export TOKEN=<YOUR_TOKEN>

Make API requests

This guide will take you through the steps you need to perform to add point values.

Add point values

To add point values, the Post values operation can be used.

Push 1 to 100 values for given point in a batch.

Only one pointValue per millisecond will be stored. PointValues are dropped if there are timestamp conflicts, i.e. if a pointValue with the same timestamp already exists. Example with following pointValues:

  • 2022-07-11T11:11:30.333
  • 2022-07-11T11:11:30.222
  • 2022-07-11T11:11:30.333
  • 2022-07-11T11:11:30.444

The first is accepted (it's the first for time "30.333"). The second is also accepted. The third is dropped because it's the same timestamp as the first. The fourth is accepted again. The indices of dropped pointValues are listed in the response (0-based), in this example there is one conflict with index "2".

If there is no conflict status 204 is returned instead of 202.

Note: Use query parameter 'overwrite=true' to force overwriting of conflicting values.

curl -X 'POST' \
  "https://eu.buildingx.siemens.com/api/openness/ingest/partitions/$PARTITION/points/$POINTID/values" \
  -H "Accept: application/vnd.api+json" \
  -H "Authorization: Bearer $TOKEN" \
  -H "Content-Type: application/vnd.api+json" \
  -d "{
  \"data\": [
    {
      \"type\": \"PointValue\",
      \"attributes\": {
        \"timestamp\": \"2000-05-11T10:32:54.964Z\",
        \"value\": \"12.66\"
      }
    }
  ]
}"

In the response, you will find the values added for the pointId.

Add point values for multiple points

To add point values for multiple points at once, use the POST /points/covs endpoint.

Push 1 time-series value for 1 to 50 points in a batch. Existing values are always overwritten.

curl -X 'POST' \
  "https://eu.buildingx.siemens.com/api/openness/ingest/partitions/$PARTITION/points/covs" \
  -H "Accept: application/vnd.api+json" \
  -H "Authorization: Bearer $TOKEN" \
  -H "Content-Type: application/vnd.api+json" \
  -d "{
  \"data\": [
    {
      \"type\": \"Point\",
      \"id\": \"$POINTID_1\",
      \"attributes\": {
        \"values\": {
          \"type\": \"PointValue\",
          \"attributes\": {
            \"timestamp\": \"2000-05-11T10:32:54.964Z\",
            \"value\": \"12.66\"
          }
        }
      }
    },
    {
      \"type\": \"Point\",
      \"id\": \"$POINTID_2\",
      \"attributes\": {
        \"values\": {
          \"type\": \"PointValue\",
          \"attributes\": {
            \"timestamp\": \"2000-05-11T10:32:54.964Z\",
            \"value\": \"22.50\"
          }
        }
      }
    }
  ]
}"

A successful request returns status 204 (No Content). If some points fail while others succeed, a 207 (Multi-Status) response is returned with details about unprocessed entries and errors.

Note

For more details on deprecation policies and common API features such as paging, filtering and errors, refer to the Developer's Guide.