The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

RESTful API for reading energy consumption and cost data for a customer.

Changelog

The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.

[1.1.1] - 2026-06-23

Added

  • Added licensedAgainstPartitionId header. When provided, quota is drawn from the subscription tied to this partition instead of any active subscription for the customer. The partition must belong to the same customer. Useful when a customer has multiple active subscriptions for the same API.

[1.1.0] - 2026-05-01

IMPORTANT CHANGES

  • API Endpoint Update: New domain and API path for the Sustainability API.
    • Old Endpoint: https://api.bpcloud.siemens.com/sustainability/v1/*
    • New Endpoint: https://eu.buildingx.siemens.com/api/openness/sustainability/v1/*
    • Action Required: Please update your integrations to use the new endpoint.
    • Grace Period: The old domain will remain available until 31 March 2027, after which it will be permanently retired.

[1.0.0] - 2026-03-01

Added

  • Release of Sustainability API.