The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

RESTful API for retrieving and managing visitor information.

Quick Start

Sample quickstart for Visitor Manager API Reference

Getting started with using Visitor Manager APIs involves the following steps:

  1. Create an account and a machine user.
  2. Create a JSON Web Token (JWT) by using the machine user credentials.
  3. Make API requests using the JWT.

Note

In the following examples we are:

  1. making use of a Linux/MacOS shell in which environmental variables are set using the export-command. In other environments it may be different, e.g. Windows uses the set-command instead.

  2. using the curl as a client. But the API can be used in any programming language with an HTTP Client, e.g. Go, Python, NodeJS, Javascript and Java.

Create an account and a machine user

The Getting Started page documents the required steps to get a hold of the clientId, clientSecret and partitionId.

Create a token

Use the values described in the Authorization- section to construct the Create Token request.

Example request

export CLIENT_ID=<YOUR_CLIENT_ID>
export CLIENT_SECRET=<YOUR_CLIENT_SECRET>

curl {{env.issUrl}} \
  -H 'content-type: application/json' \
  -d "{
            \"client_id\":\"$CLIENT_ID\",
            \"client_secret\":\"$CLIENT_SECRET\",
            \"audience\":\"{{env.audience}}\",
            \"grant_type\":\"client_credentials\"
      }"

To run this example yourself, set the CLIENT_ID and CLIENT_SECRET first.

Example response

{
  "access_token": "eyJ0eXAiOiUSJ9.eyJpc3MiOiJdGlhbHMifQ.MJpcxLfyOt",
  "token_type": "Bearer",
  "expires_in": 86400
}

The token, or JWT (JSON Web Token), is the value of the access_token-property in the response. You can now use it by passing it in the Authorization-header of any subsequent API requests. The expires_in-property represents the number of seconds your token is valid, usually, the value corresponds to 24 hours. When this time has elapsed you will need to create a new token.

Now you have all you need to start using the API. As a last step of preparation set the token and partitionId as environmental variables.

export PARTITION=<YOUR_PARTITION_ID>
export TOKEN=<YOUR_TOKEN>

Make API requests

Refer the API Reference for the available endpoints and their usage.