The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Explore our APIs. Develop innovative applications and integrations or extend the functionality of existing applications.

Authentication

This chapter aims to provide hands-on examples on how to authenticate by creation of an authorization token and making a sample call.

Example Request

Use the sample below and fill your client_id and client_secret to request an authorization token:

export CLIENT_ID=<YOUR_CLIENT_ID>
export CLIENT_SECRET=<YOUR_CLIENT_SECRET>

curl https://siemens-bt-015.eu.auth0.com/oauth/token \
  -H 'content-type: application/json' \
  -d "{
            \"client_id\":\"$CLIENT_ID\",
            \"client_secret\":\"$CLIENT_SECRET\",
            \"audience\":\"https://horizon.siemens.com\",
            \"grant_type\":\"client_credentials\"
      }"

Example Response

{
  "access_token": "eyJ0eXAiOiUSJ9.eyJpc3MiOiJdGlhbHMifQ.MJpcxLfyOt",
  "token_type": "Bearer",
  "expires_in": 86400
}

The token, or JWT (JSON Web Token), is the value of the access_token property in the response. You can now use it by passing it in the Authorization header of any subsequent API requests. The expires_in property represents the number of seconds your token is valid for, usually the value corresponds to 24 hours. When this time has elapsed you will need to create a new token.

For example, when using the Operations API to list Devices:

export TOKEN=eyJ0eXAiOiUSJ9.eyJpc3MiOiJdGlhbHMifQ.MJpcxLfyOt
export PARTITION=1bcaafc3-d4d3-43e1-ab64-89d8518d5951

curl -H "Authorization: Bearer $TOKEN" "https://eu.buildingx.siemens.com/api/openness/operations/partitions/$PARTITION/devices"

Note

Your token is valid for a limited time and your application will need to refresh it at regular intervals.

Warning

Make sure to store your token in a safe place, never share it or store it in source control. Anyone with access to your token can access the system on your behalf.