The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Explore our APIs. Develop innovative applications and integrations or extend the functionality of existing applications.

Integration Guide

This guide describes the Building X data model and walks you through the sequence of API calls needed to onboard building data. Use the accompanying Postman collection to follow along step by step.

Tip

Before you begin, make sure you have completed the Getting Started guide and have a valid access token.

Data Model

The Building X APIs are organized around a hierarchy of core resources. Understanding how they relate to each other is essential before making integration calls.

flowchart LR
    Customer -- "has" --> Partition
    Partition -- "contains" --> Location
    Device -. "has-location" .-> Location
    Equipment -. "has-location" .-> Location
    Equipment -. "is-controlled-by" .-> Device
    Equipment -. "has-equipment-type" .-> EquipmentType
    Device -- "hosts\n(point-group)" --> Point
    Equipment -- "has-points\n(point-group)" --> Point
    Point -- "has" --> PointValue
ResourceAPIDescription
CustomerAccounts APIThe company that owns the building resources, often referred to as a customer tenant.
PartitionAccounts APIA logical grouping of building data within a customer tenant. Most API calls are scoped to a partition.
LocationBuilding Structure APIA Location is the basic element describing the topological structure of a site or building, i.e. the common base class of a Campus, Building, Floor, Room etc.
DeviceBuilding Operations APIA Device can be any electronic equipment with some computing ability that has a firmware or supports the installation of software. Examples are pumps, dampers, valves, sensors, detectors, limit switches, remote/local switches or automation devices. For API integrations this typically represents a virtual data source connecting a third-party system to the platform.
EquipmentTypeBuilding Structure APIA classification of equipment (e.g. meter, sensor). Retrieved via GET /equipment-types.
EquipmentBuilding Structure APIA logical asset (e.g. an electricity meter or occupancy sensor) linked to a device, a location, and an equipment type. Equipment can form hierarchies via the isPartOf relationship.
PointBuilding Structure APIThe data interface on a device or equipment — a sensor reading, a command, or a set-point. Points are created inside a point-group scoped to a Device and then assigned to an Equipment point-group.
PointValuePoint Value Ingest APIA time-series measurement or set value for a point.

Addresses on root locations

For correct functioning of the Building X business applications, root-level locations (Campus or Building) must always have a postal address assigned via the hasPostalAddress relationship.

Data Onboarding Sequence

The diagram below shows the sequence of API calls to onboard building data, reflecting the steps in the Postman collection.

sequenceDiagram
    autonumber
    participant Client
    participant Auth as Auth Server
    participant Structure as Building Structure API
    participant Ops as Building Operations API
    participant Ingest as Point Value Ingest API

    rect rgb(240, 248, 255)
    Note over Client, Ingest: Phase 1 — Authentication
    Client->>Auth: POST /oauth/token (client_credentials)
    Auth-->>Client: access_token
    end

    rect rgb(240, 255, 240)
    Note over Client, Ingest: Phase 2 — Building Structure
    Client->>Structure: POST /locations (type: Campus + Address)
    Structure-->>Client: campusId
    Client->>Structure: POST /locations (type: Building, isBuildingOf: campusId + Address)
    Structure-->>Client: buildingId
    Client->>Structure: POST /locations (type: Floor, isFloorOf: buildingId)
    Structure-->>Client: floorId
    Client->>Structure: POST /locations (type: Room, isRoomOf: floorId)
    Structure-->>Client: roomId
    Note right of Client: Repeat for additional floors and rooms
    end

    rect rgb(255, 248, 240)
    Note over Client, Ingest: Phase 3 — Device Registration
    Client->>Ops: POST /devices (name, modelName, serialNumber)
    Ops-->>Client: deviceId
    Client->>Structure: PATCH /assets/{deviceId}/relationships/has-location
    Note right of Client: Assign device to a location (e.g. Building)
    end

    rect rgb(248, 240, 255)
    Note over Client, Ingest: Phase 4 — Equipment Setup
    Client->>Structure: GET /equipment-types
    Structure-->>Client: equipmentTypeId (e.g. "meter")
    Client->>Structure: POST /equipment (hasEquipmentType, isControlledBy: deviceId)
    Structure-->>Client: equipmentId
    Client->>Structure: PATCH /assets/{equipmentId}/relationships/has-location
    Note right of Client: Assign equipment to a location
    Note right of Client: Repeat for sub-meters (isPartOf: parent equipmentId)
    end

    rect rgb(255, 255, 240)
    Note over Client, Ingest: Phase 5 — Point Creation & Assignment
    Client->>Structure: POST /point-groups/Device-{deviceId}/points
    Structure-->>Client: pointId
    Client->>Structure: POST /point-groups/Equipment-{equipmentId}/relationships/has-points
    Note right of Client: Assign point to equipment
    Note right of Client: Repeat for each data point
    end

    rect rgb(240, 255, 255)
    Note over Client, Ingest: Phase 6 — Data Ingestion
    Client->>Ingest: POST /points/{pointId}/values (batch of timestamped values)
    Ingest-->>Client: 201 Created
    Note right of Client: Repeat for each point
    end

Phase 1 — Authentication

Obtain an access token using the client_credentials grant. See Getting Started for details.

Phase 2 — Building Structure

Create the location hierarchy using the Building Structure API. Each location type references its parent through a relationship:

  1. Campus — top-level grouping with a postal address and geo-location.
  2. Building — linked to the campus via isBuildingOf. Must also have a postal address.
  3. Floor — linked to the building via isFloorOf.
  4. Room — linked to a floor via isRoomOf.

The Postman collection creates a sample structure with one campus, one building, two floors, and two rooms per floor.

Phase 3 — Device Registration

Create a device via the Building Operations API and then assign it to a location using the Building Structure API.

For API-based integrations the device represents a virtual device — a logical data source that connects a third-party cloud system to Building X. This is different from a physical gateway device installed on-site.

Phase 4 — Equipment Setup

Equipment represents the logical assets you want to monitor (meters, sensors, etc.).

  1. Get equipment types — retrieve the available types (e.g. meter, sensor) from GET /equipment-types.
  2. Create equipment — link it to an equipment type (hasEquipmentType) and to the device (isControlledBy).
  3. Assign to a location — place the equipment at the appropriate level in the building hierarchy.
  4. Build equipment hierarchies — sub-meters or sub-sensors use the isPartOf relationship to reference a parent equipment (e.g. a floor meter is part of the building-level meter).

Phase 5 — Point Creation & Assignment

Points are the data interfaces that carry time-series values.

  1. Create points on the device — use POST /point-groups/Device-{deviceId}/points to register each data point with its name, data type, unit, and function (sensor, command, or setpoint).
  2. Assign points to equipment — use POST /point-groups/Equipment-{equipmentId}/relationships/has-points to link each point to its corresponding equipment.

Phase 6 — Data Ingestion

Push time-series values for each point using the Point Value Ingest API:

  • Single-point ingestion — POST /points/{pointId}/values with a batch of up to 100 timestamped values.
  • Multi-point batch ingestion — POST /points/covs to push 1 value for up to 50 points in a single request.

The Postman collection includes example requests for pushing electricity consumption, occupancy, and indoor air quality data.

Using the Postman Collection

The Postman collection contains ready-to-run requests organized into folders matching the phases above. It includes three scenario examples:

ScenarioEquipment TypeData Points
3.1 Energy MeterMeterElectricity consumption (kWh) at building, floor, and room level
3.2 OccupancySensorOccupancy counts per room
3.3 Indoor Air QualitySensorTemperature, humidity, CO2, TVOC, PM10, PM2.5, light, noise, NO2, CO, O3, SO2

Setup

  1. Import the collection into your tool of choice like Postman, Insomnia or Bruno.
  2. Set the following collection variables:

    VariableDescription
    API_URLThe Building X API base URL
    partitionThe partition ID to onboard data into
  3. Run the Authorize request first — it uses client_credentials to obtain a token and stores it automatically for subsequent requests.

  4. Execute the folders in order: 1. Building Structure → 2. Device → 3.x Scenario. Each request auto-saves the created resource IDs into collection variables for use in later steps.

Tip

You can run an entire folder at once by right-clicking on it in Postman and selecting Run folder.

Next Steps

  • General Information — learn about filtering, pagination, error handling, and other API conventions.
  • Try Out APIs — explore all available APIs interactively from the Developer Portal.
  • Refer to individual API overviews for detailed resource documentation.