Using the API reference
The Building X developer portal features an API Reference to document the API operations and interactions. The reference is based on Swagger UI which is a popular tool to make OpenAPI readable for developers.
To use the API Reference you need to provide a partitionId
and a valid JWT bearer token
. To get what you need, perform the following steps:
- Login to API Manager.
- Go to
Machine Users
and either pick one to use, or create a new machine user. Make sure to note down yourclientId
,clientSecret
andpartitionId
. - Create a token by using the
Generate token
action (under the context menu of your machine user) or by using the Create a Token instructions
You can now use the API Reference to make requests by opening the API Reference and providing you information as described below
- In the input box
partitionId
paste your partitionId. - Click the
Authorize
-button - Paste your token into the input box in the modal dialog, click
Authorize
, thenClose
.
You are now ready to go! To perform an API operation, open the one of your choice. Then click Try it out
, populate any required or optional input fields. Finally click Execute
.
Note
The API Reference Authorize
procedure does not actually authorize you. So it is possible to pass an invalid token at this stage. The token is checked when performing the operations. If an invalid token is provided you will receive a Not Authorized
or Forbidden
response depending on the problem.
Community
Connect and Collaborate with Industrial Professionals and Join the Community!Click to load comments