The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

REST-style, HTTP-based API used to interact with COMOS data and to access COMOS features.

Versioning and Compatibility

The COMOS Web REST API will evolve over time. Additional features will be added and existing features might be extended, adjusted or even removed. Likewise, the API clients will evolve. A client using the COMOS Web REST API might not be deployed or updated at the same time as the API. Instead, a client might be updated before the COMOS Web REST API is updated and vice versa. Different versions of a client might be used at the same time.

An older client might not know about new COMOS Web REST API features but should be able to use older features or even to detect that a feature might not be available anymore. A newer client should be able to decide which features are already supported by the COMOS Web REST API.

The API uses a versioning strategy to enable the following:

  • Both the COMOS Web REST API and the clients using the API shall be able to evolve independently to a certain extent.
  • Clients shall be able to detect existing API features during run-time and, optionally, to provide feedback on this.
    (For example, by deactivating control elements in a user interface)

Semantic Versioning

Semantic Versioning is used to version features of the COMOS Web REST API. A version number is indicated in the following format: MAJOR.MINOR.PATCH Each part is a non-negative integer consisting of digits only and without leading + or leading zeros.

Example: 1.0.5

Given a version number MAJOR.MINOR.PATCH, increment the:

  1. MAJOR version when you make incompatible API changes
  2. MINOR version when you add functionality in a backwards-compatible manner
  3. PATCH version when you make backwards-compatible bug fixes

Unsupported version numbers

Version numbers deviating from the following are not supported.

  • Version numbers for preliminary publications.
    Example: 1.0.0-alpha
  • Version numbers with build metadata.
    Example: 1.0.0+20130313144700

Keywords used

The key words "MUST", "MUST NOT", "REQUIRED", "SHALL", "SHALL NOT", "SHOULD", "SHOULD NOT", "RECOMMENDED", "MAY", and "OPTIONAL" in this document are to be interpreted as described in RFC 2119.

Versioning and client behavior

A client SHOULD implement the following behavior.

If a client has been built against a specific feature version, e.g. version 2.3.5, the following compatibility is assured:

The MAJOR version on the server is greater

  • The client MUST NOT use the server version. It MAY notify the user about this fact, e.g., by displaying a message or by deactivating or removing specific user controls.

The MAJOR version on the server is equal

  • The MINOR version on the server is greater.
    The client can use the feature and all the endpoints known to the client. The functionality of the feature has been extended since the client was implemented, but only in a compatible way.

  • The MINOR version on the server is equal.
    The client can use the feature and all the endpoints known to the client. The functionality of the feature has not changed.

  • The MINOR version on the server is smaller.
    The client can use the feature, but only the subset that has already been available up to the server version.

The MAJOR version on the server is smaller

  • The client can use the feature, but only the subset that has already been available up to the server version (including the MINOR version).

A change of the PATCH version does not affect the compatibility.

If a new MAJOR version of a feature is available, a new client implementation SHOULD adjust to the new version.

For compatibility reasons, a feature MAY be available in multiple versions temporarily, usually in the current MAJOR version and the previous MAJOR version, e.g., 1.7.3 and 2.0.1. If a feature is available in multiple versions and a client discovering the features can handle multiple versions—especially MAJOR versions—, the client SHOULD use the newer version as this is generally an improvement of the previous versions.

Example: Compatibility scenario for a client that has been built against version 2.3.5
  • The feature is available in versions 3.1.4, 2.3.5, 2.7.0 and 1.8.2. The client SHOULD use version 2.7.0. (It is compatible with 2.3.5 but newer.) It MUST NOT use version 3.1.4. (Version 3.1.4 comprises a breaking change.)
  • The feature is available in versions 2.4.7 and 2.4.8. The client SHOULD use version 2.4.8. (Both 2.4.7 and 2.4.8 are compatible with 2.3.5, but 2.3.8 is newer.)
  • The feature is available in version 3.1.4. The client MUST NOT use the available service.
  • The feature is available in version 1.4.5. The client MAY use the available service. But from a client perspective, it MAY also be valid to decide that this server version is not supported anymore.

Note

Typically, a feature will just be available in multiple MAJOR versions. Still, clients MUST be able to handle various MAJOR, MINOR or PATCH versions.

Clients MUST ignore versions with invalid version numbers

Example of invalid version numbers:

  • 1.0, 1.0.0-alpha
  • 01.0.0, a.0.0
  • 1e2.0.0, -1.0.0, 1

A client MUST be able to handle unknown additional properties — e.g., in a JSON response — without breaking if the MINOR version of the feature has increased since implementation of the client.