The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

DepotFinity is a cloud-based software service that is used to monitor, report, schedule and manage the charging operations of chargers within a depot.

RFID Management API

RFID Management API allows users to add and manage RFID cards. Enabling RFID authentication will require you to present your RFID card to start and stop charging sessions. You can also onboard multiple RFID cards in a single go.

API Usage

You must be authorized to use RFID Management API. See Token Management API for more information on how to create and use the access token.

Bulk Import RFIDs

This method allows you to insert or upload Bulk RFIDs.

Prepare Request

You can prepare the request body with parameter interimVehicleIDs in an array format. For more information, see RFID API Reference.

Request Body

{
    "interimVehicleIDs": ["YOUR_RFID"]
}

Example Request

Note

Use the server URL applicable to your region. See API Reference for available server URLs applicable to your region.

export TOKEN = <YOUR_TOKEN>
export INTERIMVEHICLEIDS = [<INTERIMVEHICLEIDS>]

curl --location --request POST 'https://api.eu.depot.emobility.io/v2/rfid' \
--header 'Content-Type: application/json' \
--header 'Accept: application/json' \
--header 'Authorization: Bearer $TOKEN' \
--data '{
        "interimVehicleIDs": $INTERIMVEHICLEIDS
    }'

Response Body

Successful response returns 201 HTTP status code with response body of RFIDImportResponse schema. For more information, see RFID API Reference.

Example Response

{
    "message": "RFID has been created successfully."
}

Status Update of a RFID

This method allows you to enable or disable RFID authentication.

Prepare Request

You can prepare the request with path parameter TAG is RFID and STATUS is boolean format. For more information, see RFID API Reference.

Example Request

export TOKEN = <YOUR_TOKEN>
export TAG = <YOUR_RFID>
export STATUS = <VALUE_STATUS>

curl --location --request POST 'https://api.eu.depot.emobility.io/v2/rfid/$TAG/$STATUS' \
--header 'Content-Type: application/json' \
--header 'Accept: application/json' \
--header 'Authorization: Bearer $TOKEN'

Response Body

Successful response returns 201 HTTP status code with response body of RFIDUpdateResponse schema. For more information, see RFID API Reference.

Example Response

{
    "message": "RFID status has been updated successfully."
}