The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

DepotFinity is a cloud-based software service that is used to monitor, report, schedule and manage the charging operations of chargers within a depot.

Token Management API

The token management API allows your application to make requests on your behalf and access data from the authorized services. For every valid request to the authorization server, an access token response for the client application is issued with the following properties.

  • access_token: Access token string issued by the authorization server.
  • expires_in: The time in seconds for which the access token is valid.
  • token_type: The type of token, typically just the string "bearer".

Note

Your token is valid for a limited time and your application will need to refresh it at regular intervals.

If the access token request is invalid, error responses are returned with the HTTP 403 status code. For detailed information on the error responses, see General Information.

Create a Token

Create a JWT (JSON Web Token) request with the Authorization header format for Token Management API.

The following sample shows the format of the Authorization header.

const CLIENT_ID=<YOUR_CLIENT_ID>;
const CLIENT_SECRET=<YOUR_CLIENT_SECRET>;

// create a base64 encoded string with CLIENT_ID and CLIENT_SECRET
const YOUR_TOKEN = Base64Encoder("${CLIENT_ID}:${CLIENT_SECRET}");

// add the authorization header
Authorization: Basic ${YOUR_TOKEN}

To run the following example, set your TOKEN.

Example Requests

Note

Use the server URL applicable to your region. See API Reference for available server URLs applicable to your region.

export TOKEN = <YOUR_TOKEN>

curl --location --request POST 'https://clientapp-auth.eu.depot.emobility.io/oauth2/token' \
  --header 'Accept: application/json' \
  --header 'Content-Type: application/x-www-form-urlencoded' \
  --header 'Authorization: Basic $TOKEN' \
  --data-urlencode 'grant_type=client_credentials'

Example Response

The access_token property in the response body is returned after the successful execution of the request. You can now pass the access_token in the Authorization header of any subsequent API requests. The expires_in property represents the number of seconds your token is valid. The token is valid for 24 hours (86400 seconds) by default. When this time has elapsed you will need to create a new token.

{
    "access_token": "eyJ0eXAiOiUSJ9.eyJpc3MiOiJdGlhbHMifQ.MJpcxLfyOt",
    "expires_in": 3600,
    "token_type": "Bearer"
}

Note

Your token is valid for a limited time and your application will need to refresh it at regular intervals.

Warning

Make sure to store your token in a safe place, never share it or store it in source control. Anyone with access to your token can access the system on your behalf.

Token Usage

Pass the access_token from the token API in the header to access DepotFinity APIs.

The following sample shows the format of the Authorization header.

export ACCESS_TOKEN = <YOUR_ACCESS_TOKEN>

# add the authorization header
Authorization: Bearer ${ACCESS_TOKEN}