Skip to content
Siemens Developer Portal

Get Area Energy Consumption

An area is a grouping of sensors on a floor. This API returns the aggregate energy consumption in watt-hour for all devices in the area for the last 15 minutes.

For example, if the request is between 10:05:00 and 10:19:59 am, energy data is sent from 9:45 to 10:00 am. Likewise, if the request is between 10:20:00 and 10:34:59, data is sent from 10:00 to 10:15 am. The data is aggregated from all fixtures in the area at 5-minute intervals and is rounded to the nearest last 15-minute interval set.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/area/v1/energy/{area_id} 

Parameters

Name Description
Request
em_ip_address_or_hostname The Manage (EM) IP address or hostname
area_id Area identifier. Use the Get All Areas API, or in EM, select Facility > Floor > Area in the left panel, and click the Settings tab to get the Area ID.
Response
energy-lighting Reports aggregate energy consumption in watt-hour for the last 15 minutes for all lighting fixtures in the area.
energy-plugload Reports aggregate energy consumption in watt-hour for the last 15 minutes for all plugloads in the area.

Sample Request

The Get All Areas API returns the list of all areas and area IDs. For example, suppose a floor has two areas: Hardware area-ID ‘9’ and Software area-ID ‘27’; the user can request Enlighted Manage to return the aggregate energy consumption in watt-hour for all devices in the Hardware area '9' for the last 15 minutes.

GET https://192.80.3.2/ems/api/org/area/v1/energy/9

Sample Response

{
  "energy-lighting": "5580.96",
  "energy-plugload": "380.63"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments