Skip to content
Siemens Developer Portal

Get all Bluetooth Fixtures by Floor

The API returns the sensor location for all BLE sensors on a floor. The data is returned as X, Y coordinates of the measured and scaled-down distance from the lower-left corner of the uploaded floor plan. The API also returns the sensor Product code.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/fixture/blefixture/list/floor/{floor_id}

Parameters

Request

Parameter Description
em_ip_address_or_hostname Manage’s IP address or hostname
floor_id Floor identifier. Use the Get All Floors API, or in EM, select Facility > Floor > in the left panel, and click the Settings tab to obtain the Floor ID.

Response

Parameter Description
id Sensor identifier.
name Sensor name. For example, Sensorxxxxxx.
x-axis Scaled reference of the distance measured in the horizontal dimension from the lower-left corner of the uploaded floor plan.
y-axis Scaled reference of the distance measured in the vertical dimension from the lower-left corner of the uploaded floor plan.
groupid Profile group identifier. The ID of the profile associated with the fixture.
macAddress MAC address.
bleMode Represents the Bluetooth Low Energy (BLE) mode of the fixture. Possible values: OFF/ON
modelNo Sensor product code. For product codes, refer to the list of Sensors and Product codes in the Spec Sheets.

Sample Request

Using the Floor ID '1' returned by the Get All Floors  API, send a request to Manage to return the x- and y-axis of the scaled-down distance from the lower-left corner of the floor plan for all BLE sensors on Floor 1.

GET https://{em_ip_address_or_hostname}/ems/api/org/fixture/blefixture/list/floor/1

Sample Response

 {

  "fixture": [

    {
      "id":   "361",
      "name":   "Sensor00c017",
      "xaxis":   "966",
      "yaxis":   "391",
      "groupid":   "185",
      "modelNo": "SU-4E-01",
      "macaddress":   "00:c0:17",
      "bleMode": "OFF"
    },
    {
      "id":   "1364",
      "name":   "Sensor0629dd",
      "xaxis":   "270",
      "yaxis":   "90",   
      "groupid":   "196",
      "modelNo": "SU-4E-01",
      "macaddress":   "06:29:dd",
      "bleMode": "OFF"
    },
    {
      "id":   "835",
      "name":   "Sensor013ec0",
      "xaxis":   "756",
      "yaxis":   "462",
      "groupid":   "55",
      "modelNo": "SU-4E-01",
      "macaddress":   "01:3e:c0",
      "bleMode": "OFF"
    }

   ]

}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments