Skip to content
Siemens Developer Portal

BLE Mode of Sensor

The API sets the BLE mode of the sensor.

Request

POST https://{em_ip_address_or_hostname}/ems/api/org/fixture/op/assignblemode/{blemode}
<fixtures> 
   <fixture>
         <id>nn</id>
   </fixture>
   <fixture>
        <id>mm</id>
  </fixture>
</fixtures>

Parameters

Request

Parameter Description
em_ip_address_or_hostname Manage’s IP address or hostname
blemode Sensor BLE mode:
- OFF – BLE mode is off;
- SCAN – The sensor scans for BLE signals;
- BEACON – The sensor sends out BLE signals.
id Sensor identifier.

Response

Parameter Description
status nnn – Number of sensors where the BLE mode was updated successfully.
msg Error message description.
-1 – Error message.

Sample Request

The example below shows how to set the BLE Mode for two sensors to the OFF mode. The response indicates that two fixtures have been updated successfully. If there is an error, the error message is displayed.

POST https://192.80.30.2/ems/api/org/fixture/op/assignblemode/OFF

Sample Response

   <fixtures>
       <fixture>
            <id>27</id>
        </fixture>
           <fixture>
                <id>28</id>
          </fixture>
    </fixtures>

  {
    "status": "2", 
  }

or

    {
      "status": "-1",
      "msg": "Error..."
    }

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments