Skip to content
Siemens Developer Portal

Get Scene Light Levels for a Switch

A Switch Group controls the light levels of selected fixtures. Each set of light level settings for fixtures is called a scene. Up to a maximum of six scenes can be created. Each fixture in a scene can have different light levels to achieve the desired effect.

The API returns the scene light levels for the group of fixtures controlled by the scene.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/scene/v1/list/getSceneLevels/{scene_id} 

Parameters

Request

Parameter Description
em_ip_address_or_hostname Manage’s IP address or hostname
scene_id Scene identifier. Returned in Get Switch Scenes API. Get Switch Scenes

Response

Parameter Description
id For internal use.
switch_id Switch identifier.
scene_id Scene identifier. Up to a maximum of six scenes can be defined.
fixture_id Fixture identifier of the fixture for which the scene applies.
lightlevel Returns the light level (0-100%) for each fixture for the scene.
- 0% - Light level is set to off.
- 100% - Light level is set to full-on.
scenecolor Current color temperature value in Kelvin degrees

Sample Request

Use the Get Switch Scenes to obtain the Scene ID. Then, request the scene light levels for the fixtures using the Scene ID. For example, if Scene ID '157' is returned by the Get Switch Scenes use the Scene ID to return the light levels for the scene.

GET https://192.80.3.2/ems/api/org/scene/v1/list/getSceneLevels/157

Sample Response

{
  "sceneLevel": [
  {
    "id": "6",
    "switchid": "7",
    "sceneid": "157",
    "fixtureid": "885",
    "lightlevel": "100",
    "sceneColor": "3200"
  },
  {
    "id": "9",
    "switchid": "7",
    "sceneid": "157",
    "fixtureid": "886",
    "lightlevel": "60",
    "sceneColor": "3600"
  }
 ]
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments