Skip to content
Siemens Developer Portal

Get the List of Emergency Fixtures by Floor

This API retrieves the fixture details and Fixture IDs for the sensors based on the designated sensor or fixture type.

Note: This API is an enhancement to the Get Sensor Location by Floor API, allowing you to filter results based on sensor type. Enlighted Manage (EM) versions below 3.10 do not support filtering based on sensor type.

The sensors in Manage are classified into the following types:

  • Emergency sensors – Returns sensors designated as emergency fixtures in the Manage (EM)
  • Desk sensors – Returns sensors designated as Desk sensors in EM. See Enable Desk Sensors.
  • Fixtureless sensors – Returns sensors designed as Fixtureless in EM including Desk sensors.
  • Fixtured sensors – Returns sensors that are not designated as fixtureless sensors.

The API response is filtered based on the category of sensors. When the category or class is not specified in the API call, the response is not filtered. If the Floor ID is incorrect, the command returns 400 with the message "Floor ID does not exist, please correct and try again".

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/fixture/location/list/floor/{floor_id}/1?class={filter}

Parameters

Request

Name Description
em_ip_address_or_hostname The Manage IP address or hostname
floor_id Floor identifier. Use the Get All Floors API, or in EM, select Facility > Floor > in the left panel, and click the Settings tab to obtain the Floor ID.
filter Filter: Class Value. Specify only one filter class, if the filter class is not specified, then the response is not filtered.
Emergency – Returns sensors designated as emergency fixtures in the Energy Manager (EM)
Desk – Returns sensors designated as Desk sensors in EM
Fixtureless – Returns sensors designed as Fixtureless in EM including Desk sensors.
Fixtured – Returns sensors that control lighting fixtures.

Response

| Name | Description | |-----------------------------|--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------| | | fixture_id | Sensor or Fixture ID. | | Fixture: | | | id | Fixture identifier | | name | Name of the Fixture | | xaxis | Scaled reference of the distance measured in the horizontal dimension from the lower-left corner of the uploaded floor plan | | yaxis | Scaled reference of the distance measured in the vertical dimension from the lower-left corner of the uploaded floor plan. | | macaddress | MAC Address. NOTE: Manage does not store leading zeros when saving or returning MAC/SNAP addresses. For example, "00:c0:17" will be stored as "0:c0:17”. | | groupid | Profile group identifier. The ID of the profile associated with the fixture. | | class | Sensor Type: Emergency, Desk, Fixtureless, Fixtured |

Sample Request

Send a request to retrieve fixture details filtered based on the type of sensors fixtured on Floor 2. The API returns the fixture details of all sensors that control light fixtures (fixtured) on Floor 2.

GET https://10.4.23.19/ems/api/org/fixture/location/list/floor/2/fixtured

Sample Response

{
  "fixtures": [
      {
          "id": "28",
          "name": "Sensor00c017",
          "xaxis": "966",
          "yaxis": "391",
          "macaddress": "0:c0:17",
          "groupid": "185",            
          "class": "fixtured"
        }
        {
          "id": "1364",
          "name": "Sensor00629dd",
          "xaxis": "270",
          "yaxis": "90",
          "macaddress": "6:29:dd",
          "groupid": "196",            
          "class": "fixtured"
        }
        {  
          "id":"17"
        }
  ]
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments