Skip to content
Siemens Developer Portal

Schedule Demand Response (DR) for all Facilities

Schedule a Demand Response (DR) for all facilities for a specific period from the start time.

Request

POST https://{em_ip_address_or_hostname}/ems/api/org/dr/scheduledr`
{
    "pricelevel": "LOW",
    "duration": "60",
    "starttime": "2015-07-21T12:15:49+05:30",
    "dridentifier": "DR16",
    "pricing": "15.0"
 }

Parameters

Request

Parameter Description
em_ip_address_or_hostname The Manage’s IP address or hostname
pricelevel DR pricing: HIGH / MODERATE / LOW / SPECIAL
duration The DR duration time in minutes (must be a whole number)
starttime Time from when DR should be in effect. Format: (yyyyMMddHHmm) year/month/day/hour/minutes
dridentifier User assigned Demand Response (DR) identifier
pricing DR pricing that is effective for the energy consumed during the DR period (optional)

Response

Parameter Description
status 0 – DR schedule successful; 1 – DR not scheduled.
msg Message description

Sample Request

Schedule a Demand Response (DR) at LOW price level for all facilities for 60 minutes starting at 5:30 am on 07-21-2015 at 15 cents. The response indicates that the DR schedule was successful.

If the user is accessing web service with proper session/authenticated token:

POST https://192.80.3.2/ems/api/org/dr/scheduledr 

Sample Response

{
  "pricelevel": "LOW",
  "duration": "60",
  "starttime": "2015-07-21T12:15:49+05:30",
  "dridentifier": "DR16",
  "pricing": "15.0"
}

{
  "status": "0",
  "msg": "DR Scheduled successful"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments