Skip to content
Siemens Developer Portal

Update Demand Response for all Facilities

Update the current running or scheduled Demand Response (DR) for all facilities.

Request

POST https://{em_ip_address_or_hostname}/ems/api/org/dr/updatedr
{
    "pricelevel": "LOW",
    "duration": "60",
    "starttime": "2015-07-21T12:15:49+05:30",
    "dridentifier": "DR16",
    "pricing": "15.0"
 }

Parameters

Request

Name Description
em_ip_address_or_hostname The Manage’s IP address or hostname
pricelevel DR pricing: HIGH/ MODERATE/ LOW/ SPECIAL
duration The DR duration time in minutes (must be a whole number)
starttime Time from when DR should be in effect. Format: (yyyyMMddHHmm) year/month/day/hour/minutes. For example, 2015-11-18T17:43:00
dridentifier DR identifier provided at the time of scheduling
pricing DR pricing that is effective for the energy consumed during the DR period (optional)

Response

Name Description
status 0 – DR schedule successful
1 – DR not scheduled
msg Message description

Sample Request

Update the currently running Demand Response (DR) from LOW to HIGH price level for all facilities for 60 minutes starting at 5:30 am on 07-21-2015 at 15 cents. The response indicates that the DR update was successful.

If the user is accessing web service with proper session/authenticated token:

POST https://{192.80.30.2}/ems/api/org/dr/updatedr

Sample Response

{
    "pricelevel": "HIGH",
    "duration": "60",
    "starttime": "2015-07-21T12:15:49+05:30",
    "dridentifier": "DR16",
    "pricing": "15.0"
}

{
    "status": "0",
    "msg": "DR updated successfully"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments