Skip to content
Siemens Developer Portal

Get All Fixtures by Area

The API returns the location for all fixtures in an area on a floor. An area is a grouping of sensors or fixtures on a floor. The data is returned as X, Y coordinates of the measured and scaled-down distance from the lower-left corner of the uploaded floor plan.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/fixture/v1/location/list/area/{area_id}

Parameters

Request

Name Description
em_ip_address_or_hostname The Enlighted Manage (EM) IP address or hostname
area_id Area identifier. Use the Area ID returned in the Get All Areas API, or in EM, select Facility > Floor > Area in the left panel, and click the Settings tab to obtain the Area ID.

Response

Name Description
id Sensor identifier.
name Sensor name. For example, Sensorxxxxxx.
xaxis Scaled measurement of distance in the horizontal dimension from the lower-left corner of the uploaded floor plan.
yaxis Scaled measurement of distance in the vertical dimension from the lower-left corner of the uploaded floor plan.
macaddress Sensor's MAC address. NOTE: Manage does not store leading zeros when saving or returning MAC/SNAP addresses. For example, "00:c0:17" will be stored as "0:c0:17”.
groupid Light Profile identifier. The ID of the profile associated with the fixture.

Sample Request

Request the x- and y-axis coordinates for all sensors in the area with ID ‘9’.

GET https://192.80.3.2/ems/api/org/fixture/v1/location/list/area/9

Sample Response

{
  "fixture": [
    {
      "id": "361",
      "name": "Sensor00c017",
      "xaxis": "966",
      "yaxis": "391",
      "macaddress": "0:c0:17",
      "groupid": "185"
    },
    {
      "id": "1364",
      "name": "Sensor0629dd",
      "xaxis": "270",
      "yaxis": "90",
      "macaddress": "6:29:dd",
      "groupid": "196"
    },
    {
      "id": "835",
      "name": "Sensor013ec0",
      "xaxis": "756",
      "yaxis": "462",
      "macaddress": "1:3e:c0",
      "groupid": "55"
    }
  ]
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments