Skip to content
Siemens Developer Portal

Get Sensor Energy Consumption

Reports energy consumed in watt-hour for the last 15 minutes by the fixture.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/fixture/v1/energy/{fixture_id}

Parameters

Request

Name Description
em_ip_address_or_hostname The Manage IP address or hostname
fixture_id The fixture or sensor identifier. Use the Fixture ID returned in the Get Sensor Details by Floor API or in EM, select Facility > Floor in the left panel, Floor Plan tab, and double-click the fixture icon in the floor plan to obtain the Fixture ID.

Response

Name Description
energy Reports energy consumed in watt-hour for the last 15 minutes by the lighting fixture

Sample Request

Send a request using the Fixture ID returned by the Get Sensor Details by Floor API to return the energy consumed in watt-hour for the last 15 minutes.

GET https://192.80.3.2/ems/api/org/fixture/v1/energy/28

Sample Response

{
  "energy": "50.96"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments