Skip to content
Siemens Developer Portal

Get Sensor Energy Consumption by Area

Returns the aggregate energy consumed in watt hour by all fixtures in the area for the last 15 minutes.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/fixture/v1/energy/area/{area_id}

Parameters

Name Description
Request
em_ip_address_or_hostname The Manage IP address or hostname
area_id Area Identifier. Use the Area ID returned in the Get All Areas API, or in EM, select Facility > Floor in the left panel, and click the Settings tab to get the Area ID.
Response
energy Reports aggregate energy consumed in watt-hour for the last 15 minutes by the lighting fixtures in the area

Sample Request

Send a request to Enlighted Manage using the Area ID returned by the Get All Areas API. The API returns the energy consumed in watt-hour for the last 15 minutes for all fixtures in the area.

GET https://192.80.3.2/ems/api/org/fixture/v1/energy/area/9

Sample Response

{
  "energy": "250.96"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments