Skip to content
Siemens Developer Portal

Get All Buildings API

Retrieve the list of all buildings on the campus for the organization, including the Building ID and Building details.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/building/list/{campus_id}

Parameters

Request

Name Description
em_ip_address_or_hostname The Enlighted Manage (EM) IP address or hostname
campus_id The ID of the campus for which all buildings will be returned

Response

Name Description
id Building identifier from Manage
name Building name as described in Manage
useOrgLocation For internal use
visible For internal use
useOrgLocationTz For internal use
energySaveCalcMethod Energy savings calculated based on the sensor’s baseline energy or contract baseline energy.
SENSOR_BASED – Savings based on the sensor’s baseline energy
CONTRACTUAL – Savings based on contract baseline energy. The contract baseline energy is calculated using the annual baseline energy savings stipulated in the customer’s signed agreement for the campus at the time of installation.
contractBaseline Baseline energy savings for the campus

Sample Request

Send a GET request to return the list of all buildings for the campus ID. Details are returned as an object response if a single building is available on the campus. If more than one building is available on the campus, details are returned as an array response.

In the example below, the campus has a single building called ‘Main Building’ and its details are returned as shown.

GET https://192.80.3.2/ems/api/org/building/list/3

Sample Response

{
   "building": {
       "id": "4",
       "name": "Main Building",
       "useOrgLocation": "true",
       "visible": "true",
       "useOrgLocationTz": "true",
       "energySaveCalcMethod": "SENSOR_BASED",
       "contractBaseline": "0.00"
   }
}

When a campus has two buildings: ‘Main 5’ and 'Main 6', their details are returned as shown below.

 GET https://192.80.3.2/ems/api/org/building/list/4
{
   "building": [
  {
       "id": "5",
       "name": "Main 5",
       "useOrgLocation": "true",
       "visible": "true",
       "useOrgLocationTz": "true",
       "energySaveCalcMethod": "SENSOR_BASED",
       "contractBaseline": "0.00"
   },
   {
       "id": "6",
       "name": "Main 6",
       "useOrgLocation": "true",
       "visible": "true",
       "useOrgLocationTz": "true",
       "energySaveCalcMethod": "SENSOR_BASED",
       "contractBaseline": "0.00"
   }
]
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments