Skip to content
Siemens Developer Portal

Get Plugload Controller Energy Consumption API

The API returns managed and unmanaged energy consumed in watt-hour for the last 15 minutes by the Plug Load Controller (PLC).

For example, if the request has been sent between 10:05:00 and 10:19:59 am, energy data is sent for the period from 9:45 to 10:00 am. Likewise, if the request is between 10:20:00 and 10:34:59, data is sent for the period from 10:00 to 10:15 am. The data is aggregated from the PLC at 5-minute intervals and is rounded to the nearest last 15-minute interval set.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/plugload/v1/energy/{plugload_id}

Parameters

Name Description
Request
em_ip_address_or_hostname The Manage IP address or hostname.
plugload_id Plug Load identifier. Use the PLC ID returned in the Get All Plugloads by Floor API, or in Enlighted Manage, select Facility > Floor in the left panel, Floor Plan tab, and double-click the Plug Load icon on the floor plan to obtain the Plug Load ID.
Response
managed-energy Reports managed energy consumption in watt-hour by the PLC.
unmanaged-energy Reports unmanaged energy consumption in watt-hour by the PLC.

Sample Request

Send a request to the EM using the Plug Load ID ‘361’ returned by the Get All Floors API to return the energy consumed in watt-hour for the last 15 minutes by the PLC.

GET https://192.80.3.2/ems/api/org/plugload/v1/energy/46

Sample Response

{
  "managed-energy": "50.96",
  "unmanaged-energy": "5.4"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments