Skip to content
Siemens Developer Portal

Get Plugload Energy Consumption by Area API

Returns the aggregate managed and unmanaged energy consumed in watt-hour by all plugloads in the area for the last 15 minutes.

For example, if the request has been sent between 10:05:00 and 10:19:59 am, energy data is sent for the period from 9:45 to 10:00 am. Likewise, if the request is between 10:20:00 and 10:34:59, data is sent for the period from 10:00 to 10:15 am. The data is aggregated from all plugloads at 5-minute intervals and is rounded to the nearest last 15-minute interval set.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/plugload/v1/energy/area/{area_id}

Parameters

Name Description
Request
em_ip_address_or_hostname The Manage IP address or hostname.
area_id Area Identifier. Use the Area ID returned in the Get All Areas API, or in EM, select Facility > Floor in the left panel, and click the Settings tab to obtain the Floor ID.
Response
managed energy Reports aggregate managed energy consumption in watt-hour by all the plugloads in the area.
unmanaged energy Reports aggregate unmanaged energy consumption in watt-hour by all the plugloads in the area.

Sample Request

Send a request to the EM using Area ID '9' returned by the Get All Areas API to return the energy consumed in watt-hour for the last 15 minutes by all plugloads in the area.

GET https://192.80.3.2/ems/api/org/plugload/v1/energy/area/9

Sample Response

{
  "managed-energy": "150.96",
  "unmanaged-energy": "15.4"
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments