Skip to content
Siemens Developer Portal

Get All Plugloads by Area

The API returns plugload location for all plugloads in an area. The data is returned as X, Y coordinates of the measured and scaled-down distance from the lower-left corner of the uploaded floor plan.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/plugload/v1/location/list/area/{area_id}/1

Parameters

Request

Name Description
em_ip_address_or_hostname The Manage IP address or hostname.
area_id Area identifier. Use the Area ID returned in the Get All Areas API, or in EM, select Facility > Floor in the left panel, and click the Settings tab to obtain the Area ID.

Response

Name Description
id Plugload identifier.
xaxis Scaled measurement of distance in the horizontal dimension from the lower-left corner of the uploaded floor plan.
yaxis Scaled measurement of distance in the vertical dimension from the lower-left corner of the uploaded floor plan.
macaddress Plugload MAC address. NOTE: Manage does not store leading zeros when saving or returning MAC/SNAP addresses. For example, "00:c0:17" will be stored as "0:c0:17”.
groupid Profile group identifier. The ID of the profile associated with the plugload.

Sample Request

For example, the Get All Areas API returned two areas: Hardware area with ID ‘9’ and Software area with ID ‘27’. Request the EM for the x- and y- coordinates of the scaled-down distance of the floor plan for all plugloads in the area with area ID ‘9’.

GET https://192.80.3.2/ems/api/org/plugload/v1/location/list/area/9/1

Sample Response

{
  "plugload": [
    {
      "id": "361",
      "name": "Plugload00c017",
      "status": "0",
      "xaxis": "966",
      "yaxis": "391",
      "macaddress": "0:c0:17",
      "groupid": "185",
    },
    {
      "id": "1364",
      "name": "Plugload0629dd",
      "status": "1",
      "xaxis": "270",
      "yaxis": "90",
      "macaddress": "6:29:dd",
      "groupid": "196",
    },
    {
      "id": "835",
      "name": "Plugload013ec0",
      "status": "0",
      "xaxis": "756",
      "yaxis": "462",
      "macaddress": "1:3e:c0",
      "groupid": "55",
    }
  ]
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments