Skip to content
Siemens Developer Portal

Get Plugload Details API

The API returns the plugload details.

Request

GET https://{em_ip_address_or_hostname}/ems/api/org/plugload/v1/details/{plugload_id}

Parameters

Request

Name Description
em_ip_address_or_hostname The Enlighted Manage (EM) IP address or hostname.
plugload_id Plugload identifier. Use the Plugload ID returned in the Get All Plugloads by Floor, or in EM, select Facility > Floor in the left panel, Floor Plan tab, and double-click the plugload icon on the floor plan to obtain the Plugload ID.

Response

Name Description
id Plugload identifier.
xaxis Scaled measurement of distance in the horizontal dimension from the lower-left corner of the uploaded floor plan.
yaxis Scaled measurement of distance in the vertical dimension from the lower-left corner of the uploaded floor plan.
location Location of the plugload in the building.
floorId Floor identifier.
campusid Campus identifier.
buildingid Building identifier.
macaddress Plugload MAC address. Note: Manage does not store leading zeros when saving or returning MAC/SNAP addresses. For example, "00:c0:17" will be stored as "0:c0:17”.
version Plugload version number.
voltage Plugload voltage.
active true – Plugload working. false – Plugload not working.
Ignore the remaining parameters displayed

Sample Request

Using the Plugload ID ‘361’ returned by the Get All Plugloads by Floor API, request EM for plugload details. The response includes the plugload details for the plugload.

GET https://192.80.3.2/ems/api/org/plugload/v1/location/list/floor/1/1

Sample Response

{

  "plugload": [

    {
      "id": "361",
      "name": "Plugload00c017",
      "status": "0",
      "xaxis": "966",
      "yaxis": "391",
      "macaddress": "0:c0:17",
      "groupid": "185"
    },
    {
      "id": "364",
      "name": "Plugload0629dd",
      "status":"1",
      "xaxis": "270",
      "yaxis": "90",
      "macaddress": "6:29:dd",
      "groupid": "196"
    },
    {
      "id": "835",
      "name": "Plugload013ec0",
      "status":"0",
      "xaxis": "756",
      "yaxis": "462",
      "macaddress": "1:3e:c0",
      "groupid": "55"
    }
  ]
}

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments