Skip to content
Siemens Developer Portal

Change Color

The API changes the color temperature of the Tunable White fixtures to a specified setting for the specified duration.

Request

POST https://{em_ip_address_or_hostname}/ems/api/org/sensor/tunable-white/change-color/value/{target_color_value}/{time}
<fixtures>
  <fixture>
   <id>63</id>
  </fixture>
  <fixture>
    <id>145</id>
  </fixture>
</fixtures> 

Parameters

Name Description
Request
em_ip_address_or_hostname Manage IP address or hostname
target_color_value Color Temperature in Kelvin degrees.The valid range depends on the Fixture Manufacturer Table (FMT) supplied by the manufacturer for the fixture.
time Duration in minutes
Response
status If the request is successfully handled “Change color success” message is displayed. When sensor details are missing or inaccurate in the Post command, “Sensors list is empty while requesting API” message is displayed.

Sample Request

Change the color temperature value to 3200 for 60 minutes using the Fixture ID. The response ‘Change color success’ indicates that the color change is successfully applied to the Tunable White fixtures. Note that the response is a group response for all fixtures. The response is reported as a success if the message is successfully sent to the sensors.

POST https://10.8.1.90/ems/api/org/sensor/tunable-white/change-color/value/3200/60
<fixtures>
  <fixture>
   <id>63</id>
  </fixture>
  <fixture>
    <id>145</id>
  </fixture>
</fixtures> 

Sample Response

<?xml version="1.0" encoding="UTF-8" standalone="yes"?>
   <response>
      <status>0</status>
      <msg>change color success</msg>
   </response> 

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments