Fetch a Tag¶
Retrieves a Tag’s properties based on its Tag ID.
Request¶
GET /api/v1/enterprises/<enterprise_id>/tags/<tag_id>
Parameters¶
Request¶
Name | Value | Description |
---|---|---|
enterprise_id | string | The ID of the organization |
tag_id | string | The ID or MAC address of the tag that is being queried. Scan the QR code on the tag to get the Tag_ID and the MAC address. |
Response¶
Name | Value | Description |
---|---|---|
tag_id | string | The ID or MAC address of the tag that is being queried. Scan the QR code on the tag to get the Tag_ID and the MAC address. |
tagID | string | The ID of the tag that is queried |
tagMAC | string | MAC address of the tag |
zone | string | Zone assigned to the tag |
floor | string | Zone assigned to the tag |
motion | string | true – The tag is moving |
false – The tag is not moving | ||
displayCoordinates | string | Coordinates of the marker to be displayed for the tag. The coordinates of the tag’s path are translated left and up by the anchor’s x and y points. Note that this does not indicate the actual position of the tag. |
rawDataTimestamp | string | Timestamp of the most recent raw data included in the computation of this tag position |
computationTimestamp | string | Timestamp at which this position was computed |
batteryVoltage | string | Tag voltage |
batteryVoltageTimestamp | string | Timestamp of the latest battery voltage update |
buttonStatus | string | Tamper: When an Asset Tag is removed from an asset, the Tag’s Tamper button gets activated. |
true – Tamper Button on the Asset Tag is activated | ||
false – Tamper Button is not activated | ||
Attention: Tag button events when the attention button is activated on the physical tag | ||
true – Attention Button on the Asset Tag is activated | ||
false – Attention Button is not activated | ||
buttonTimeStamp | String | Timestamp of the most recent button message received from the tag |
Sample Request¶
GET /api/v1/enterprises/211/tags/11
Sample Response¶
{
"tagId": "da375073-7e33-480d-8209-3467c6ccbc1b",
"tagMac": "6864F5AD2C04",
"zone": "Scrum_Area",
"floor": "AAVmbG9vcgACdXMA7sxRX-kR6qQSr2ZiKK_pyL7WMV_pEeq0LVf43pYdWg",
"motion": false,
"displayCoordinates": {
"x": 0.0,
"y": 0.0
},
"rawDataTimestamp": "2022-11-15T07:38:25+00:00",
"computationTimestamp": "2022-11-15T07:38:29.889260+00:00",
"batteryVoltage": 2.823,
"batteryVoltageTimestamp": "2022-11-15T07:42:15+00:00",
"buttonStatus": {
"tamper": true,
"attention": false
},
"buttonTimestamp": "2022-11-15T07:38:54+00:00"
}
Community
Connect and Collaborate with Industrial Professionals and Join the Community!Click to load comments