The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

The Enlighted lighting solution optimizes energy savings while enhancing occupant productivity, well-being, and security.

Getting Started

The Streaming API uses the same Authentication & Authorization mechanisms as the RTLS API. Simply follow the instructions here and provide the same Authorization and x-dsp-selected-tenant-role headers when establishing the websocket connection.

To ensure that a client’s credentials remain valid for the duration of the connection, clients will have to update their credentials at a regular cadence, or they will be disconnected. See the refreshCredentials command and refreshSuccess event for more details on how to keep the credentials up-to-date.

The Location Intelligence APIs use Machine-to-Machine Authentication and Authorization with OAuth2.0 client credentials flow.

End-user requests Enlighted for API access.

Once approved, Enlighted will email the end-user with a Client ID and Client Secret.

Request Auth0 service for a Bearer token using a Client ID and Secret provided by Enlighted.

Example request for Bearer Token

curl --request POST \
--url https://enlightedinc-p01.us.auth0.com/oauth/token \
--header 'content-type: application/json' \
 --data '{"client_id":<client_id>,"client_secret":<client_secret>,"audience":"https://rtls-us-east-1-prod.dsp.enlightedinc.com","grant_type":"client_credentials"}'

Response

{
   "access_token": <access_token>,
   "token_type": "Bearer"
 }

Connection parameters

The following parameters can be provided as query string parameters when establishing the connection to the streaming API in order to control the connection:

ParameterTypeDefaultNotes
enterpriseIdintN/AThe ID of the enterprise to subscribe to data for. Must be provided
floorsstring (can be provided multiple times to select multiple options)N/ASet of floors to subscribe to data from. If not provided, no filtering is applied
eventTypesstring (can be provided multiple times to select multiple options)All event types except floorExitThe eventTypes to subscribe to
tagHeartbeatIntervalint (must be between 300 and 86400)14395How frequently (in seconds) to receive tagHeartbeat messages