The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

The Enlighted lighting solution optimizes energy savings while enhancing occupant productivity, well-being, and security.

Location Services (RTLS) APIs

Location Services REST APIs

The Location Intelligence (LI) APIs, accessible through RESTful HTTP APIs, provide seamless interaction with asset and badge tags. These tags are tracked within the Location Intelligence system using their BLE capabilities and the Enlighted sensors. The APIs facilitate real-time tracking and monitoring of tag movement, triggering events based on configured conditions. Physical asset tags are equipped with attention and tamper buttons, that allow for events to be triggered from the tags. Users have the flexibility to configure Bluetooth tag settings directly through the APIs, allowing them to set reporting intervals and select sensors strategically to optimize network performance. The functionalities supported by the APIs include fetching individual tags, iterating over all tags, and conducting connectivity tests for a comprehensive user experience.

Location Services Streaming APIs

The Location Intelligence Streaming API uses real-time data retrieval by allowing clients to establish a connection that provides updates only when changes occur. Instead of relying on traditional polling requests, this API continuously queries and promptly delivers information as events unfold. This functionality is especially beneficial in scenarios like RTLS, where immediate awareness of events, such as button presses, is crucial. The Streaming API not only offers real-time data but also a diverse array of events, data types, and commands to facilitate seamless tracking and monitoring. By optimizing the management and tracking of tagged objects, this API becomes an invaluable resource for enhancing space utilization and efficiency.

Features:

  • Monitor the real-time motion of tagged objects within a space.
  • Effortlessly access detailed data on battery status, location, and various attributes of tracked objects.
  • Harness the power of commands to request specific information, ensuring the status of connected devices.
  • Utilize secure connections and user authentication to protect data integrity and control access.
  • Leverage location optimization for improved decision-making based on real-time location data.