The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

The Enlighted lighting solution optimizes energy savings while enhancing occupant productivity, well-being, and security.

Getting Started

In Manage, users are assigned to a user role and a facility for greater control and security. When a user is assigned to a facility, the user can only issue API calls for the assigned facility and role permissions. A role grants the user the ability to perform specific tasks. You can manage roles and assign facilities to a user in the User Management section in the Manage Administration menu.

When an API request is made, if the user role provides permission to the requested API and the user has access to the assigned facility, the request will be authorized and allowed to be completed. For example, users can request data from the sensors on the floor or area in the facility to which they have access. The API call returns a permission error if the user does not have access to the facility or permission to view data.

API Authentication for Manage v4.5 and Above

Users must be authenticated to send or receive API requests to and from Manage. For authentication, send the following headers along with the REST API.

Generating the API Key

To generate an API key for a user, see Generate API Key.

For API authentication, send the following Headers along with the REST API call:

  • UserId – username
  • Authorization – Generated API key copied from the Manage application.

For example, a user is assigned the following values:

  • UserId: bob
  • Authorization: apikey e511c7a4b04740f2f3c519209ad7429ac3f9f728b97c5d8cd1c88096987ad0d1

API Example

>curl -s --get -H "UserId: **bob**" -H "Authorization:   
apikey **e511c7a4b04740f2f3c519209ad7429ac3f9f728b97c5d8cd1c88096987ad0d1**" -H   
"Accept:  application/json" -k "http://localhost:8080/ems/api/switch-groups?facility=FLOOR&facilityId=5" -v -k  
*   Trying 127.0.0.1:8080...  
* Connected to localhost (127.0.0.1) port 8080 (#0)  
> GET /ems/api/switch-groups?facility=FLOOR&facilityId=5 HTTP/1.1  
> Host: localhost:8080  
> User-Agent: curl/7.83.1  
> UserId: bob  
> Authorization: apikey e511c7a4b04740f2f3c519209ad7429ac3f9f728b97c5d8cd1c88096987ad0d1  
> Accept:  application/json  
> 

Note: Ensure that the API key and other credentials are entered in the request Header.

API Authentication for Manage v4.4 and Below

Users must be authenticated to send or receive API requests to and from Manage. For authentication, send the following headers along with the REST API.

  • API key – Unique identifier for the user (this is the user name, for example, Bob and the generated API key copied from Manage).
  • Timestamp - Time, date, and day of the API call. This is included to avoid replay attacks.
  • Authorization - SHA-1 authorization key (Calculated using the API key and timestamp).

Generating the API Key

To generate an API key for a user, see Generate API Key. Then, determine the timestamp (ts), authorization token as explained below, and send the headers along with the REST API call.

For example, user Bob is assigned the following values:

  • Username: bob
  • API Key: 6eb6f07fd09b18dd61dd353dfb669820e7859cd3 (Copied from Manage)

Time Stamp and SHA-1 Authorization

Calculate timestamp and SHA-1 authorization values for the user as follows:

  1. Use the formula below to calculate timestamp (ts):

    ts=echo $(($(date +%s%N)/1000000))

    For example, if today's GMT date and time is Thursday, March 3,  2016, 7:36:51.032 PM, the timestamp will be 1457033811032

    ts: 1457033811032

  2. Use the following command to calculate SHA-1 authorization in Linux:

SHA1="$(echo -n "$username$apikey$ts" | sha1sum -t | awk '{print $1}')".
  • Authorization: e20ac2c963ccfacf23a1f70287286443820e66d1

For API authentication, send the following Headers along with the REST API call:

  • APIkey: bob (Note: The APIkey here is the username)

  • Authorization: e20ac2c963ccfacf23a1f70287286443820e66d1

  • ts: 1457033811032  

API Example

:~$ curl -s --get -H "ApiKey:  bob" -H "Authorization: 
e20ac2c963ccfacf23a1f70287286443820e66d1" -H "ts:1457033811032" -H "Accept: 
application/xml" -H "Content-Type: application/xml" -k 
https://em_ip_address/ems/api/org/em/v1/energy -v -k
 * Hostname was NOT found in DNS cache
 *   Trying 127.0.0.1...
 * Connected to localhost (127.0.0.1) port 443 (#0)
 * successfully set certificate verify locations:
 *   CAfile: none
   CApath: /etc/ssl/certs
 * SSLv3, TLS handshake, Client hello (1):
 * SSLv3, TLS alert, Client hello (1):
 * SSLv3, TLS handshake, Server hello (2):
 * SSLv3, TLS handshake, CERT (11):
 * SSLv3, TLS handshake, Server key exchange (12):
 * SSLv3, TLS handshake, Server finished (14):
 * SSLv3, TLS handshake, Client key exchange (16):
 * SSLv3, TLS change cipher, Client hello (1):
 * SSLv3, TLS handshake, Finished (20):
 * SSLv3, TLS change cipher, Client hello (1):
 * SSLv3, TLS handshake, Finished (20):
 * SSL connection using ECDHE-RSA-AES256-GCM-SHA384
 * Server certificate:
 * subject: C=US; ST=California; L=Sunnyvale; O=Enlighted Inc.; OU=Manage
 * start date: 2015-12-15 06:37:22 GMT
 * expire date: 2040-12-08 06:37:22 GMT
 * issuer: C=US; ST=California; L=Sunnyvale; O=Enlighted Inc.; OU=Manage
 * SSL certificate verify result: self signed certificate (18), continuing anyway.
 > GET /ems/api/org/facility/v1/energy/1 HTTP/1.1
 > User-Agent: curl/7.35.0
 > Host: localhost
 > ApiKey:  bob
 > Authorization: e20ac2c963ccfacf23a1f70287286443820e66d1
 > ts:  1457033811032
 > Accept: application/xml
 > Content-Type: application/xml
 >
 < HTTP/1.1 200 OK
 < Date: Thu, 03 Mar 2016 19:42:55 GMT
 * Server Apache-Coyote/1.1 is not blacklisted
 < Server: Apache-Coyote/1.1
 < Content-Type: application/xml
 < Content-Length: 234
 < Set-Cookie: JSESSIONID=8CE1F42FCBCCEE5AB69175D45673951F; Path=/ems/; HttpOnly
 < Via: 1.1 127.0.0.1
 < Vary: Accept-Encoding