The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

API Error Reporting Guidelines

Introduction

Our goal is to harmonize the reporting of errors for API clients. The representation of an error should be no different than the representation of any resource, just with its own set of fields. In addition to use HTTP error codes, which are often too coarse to guide the API client to solve the problem, we apply an extensible approach for the possible wide range of error types. This set of rules harmonizes all APIs reporting errors to API clients. The interoperability of the format reduces efforts for the API producer as well as on the API client side.

Most of the time in development is spent for reading and understanding the code. Therefore, a fast understanding of reported errors of an API is very important. The API error guidelines assure that enough information to handle client-side and server-side errors in a consistent way such as unauthorized, retry timespans, or a maximum of calls per timespan will be provided and the developers of the API clients have a consistent way to handle reported errors simpler.

This page provides guidance on how an API developer must implement an error handling approach to handle reported errors of the APIs. If the API reports errors as it is covered in this page, an API client is able to inspect the error and find an appropriate solution.

API MUST use official HTTP status codes as intended [300]

An API MUST consistently use official HTTP status codes only with their intended semantics. The official HTTP status codes are defined and registered at:

The rule 301 lists the supported error codes. The different 4xx HTTP status codes are used for errors caused by API client side and 5xx HTTP status codes reports server side errors.

API SHOULD only use most common HTTP status codes [301]

An API SHOULD use the most commonly used codes as these are best understood. You SHOULD avoid less commonly used codes or own error codes that may create misconceptions and misunderstandings due to less familiar semantics. If the API has to report a HTTP error code which is not covered in the list below, the API specification MUST define the semantic of the error code.

Response codes MUST be documented in the API documentation, if the API reports or supports these error types. The official HTTP status codes are grouped in the following four classes. These HTTP status codes need to be used consistently with their intended semantics as per the RFC standards.

No extensions to cited RFC

The following status codes are not changed to the referenced RFC 9110 and RFC 6585. These status codes are listed to provide you a comprehensive, self-contained and complete overview of the most used HTTP status codes. The RFCs and IANA offer more status codes but these are not common for REST API and you should use them consciously and carefully only.

Client Error 4xx Status Codes [301.3]

CodeResponse                                                                                                           DescriptionMethods
400Bad RequestThe request could not be processed by the server because the request is perceived as client error (such as, malformed request syntax, invalid request message framing, or deceptive request routing). The API client MUST change its request to proceed.all
401UnauthorizedThe API client is not providing valid authentication credentials for the target resource. The server generating a 401 response MUST send a WWW-Authenticate header field containing at least one challenge applicable to the target resource.
If the request included authentication credentials, then the 401 response indicates that authorization has been refused for those credentials (such as, expired token).
all
403ForbiddenThe API client is not allowed to access the resource. The API client SHOULD not repeat the request.
In contrast to error code 401 the server understood the request and the provided authentication credentials, but refuses to authorize the API client.
Only use if user has read access, otherwise always use 404 for security reasons to hide the existence of resource.
POST, PUT, PATCH, DELETE
404Not FoundThe resource is not found. The service did not find a current representation for the target resource or is not willing to disclose that one exists. A 404 status code does not indicate whether this lack of representation is temporary or permanent; the 410 (Gone) status code is preferred over 404 if the origin server knows, presumably through some configurable means, that the condition is likely to be permanent.all
405Method Not AllowedThe method received in the request-line is known by the origin server but not supported by the target resource. The service MUST generate an Allow header field in a 405 response containing a list of the target resource's currently supported methods.all
406Not AcceptableThe service is not able or willing to respond using the request media-type or representation asked by the API client in the Accept header. The server SHOULD generate a payload containing a list of available representation characteristics and corresponding resource identifiers from which the user or user agent can choose the one most appropriate.all
408Request TimeoutThe request timed out because a server did not respond within the expected waiting time. A server SHOULD send the "close" connection option in the response, since 408 implies that the server has decided to close the connection rather than continue waiting. Note this response is often generated on gateways in the communication path.all
409ConflictThe request is not executed because of a conflict with the current state of the target resource, such as concurrent or duplicate request. The API client needs to decide how to continue, but it is expected that the API client is able to resolve the conflict to proceed.POST, PUT, PATCH, DELETE
412Precondition FailedThe request failed to process because the service evaluated the conditions given in the request header to false, such as If-Match conditions for optimistic locking.
The response status code allows the API client to place preconditions on the current resource state (its current representations and metadata) and, thus, prevent the request method from being applied if the target resource is in an unexpected state.
PUT, PATCH, DELETE
415Unsupported Media TypeThe request body (payload) is in a format or media type that the server does not support. The format problem might be due to the request's indicated Content-Type or Content-Encoding, or as a result of inspecting the data directly.POST, PUT, PATCH, DELETE
429Too Many RequestThe API client has sent too many requests in a given timespan. The response SHOULD include details explaining the condition. The response SHOULD include the Retry-After header field indicating how long to wait before making a new request.all

Server Error 5xx Status Codes [301.4]

CodeResponse                                               DescriptionMethods
500Internal Server ErrorAn unexpected error occurred and the server is not fulfilling the request. Please consider the NOT Expose Stack Traces of Your Error rule.all
501Not implementedThe server is not supporting the request. This is the appropriate response when the server does not recognize the request method and is not capable of supporting it for any resource. Return status code 405 has preference over 501.all
503Service UnavailableThe service is temporary not available due to overload or maintenance. The server MAY return the Retry-After header to suggest an appropriate time to wait for the API client before retrying the request, for example, the maintenance window ends in x minutes.all

API SHOULD use most specific HTTP status code for error [302]

An API SHOULD use the most specific HTTP status code when returning information about the request processing state or reported error situations.

API SHOULD not expose stack traces [303]

An API reports errors, but it SHOULD NOT expose stack traces. Firstly, stack traces are not part of an API specification, secondly API clients should never rely on stack traces to change a request. Moreover, stack traces expose sensitive information of the code and its dependencies that partners and third parties are not allowed to receive and may disclose unintended insights about vulnerabilities to attackers.

Additionally, the other properties of a JSON error object can expose sensitive information of the code and its dependencies. Therefore the reported errors SHOULD be evaluated in a threat and risk analysis if the reported information offers an attack vector on the Xcelerator service.

API SHOULD report problems with an errors object [304]

Errors SHOULD be described in the error objects. In the response, the top level member is the errors object for API. The errors collection MUST not be empty but contain at least one error object.

With the error object, the raised problem is communicated to the API client to react accordingly. errors are intended to explain 4xx or 5xx HTTP status codes in more detail. The errors collection SHOULD report all known and identified problems from the API to the API client. The list of errors contains all known occurred errors on the backend. The objective is to avoid a step-wise exploration of issues until all are fixed. Of course in case of a distributed system not all errors are known in advance, but what could be validated, SHOULD be reported to the API client.

Error object SHOULD be represented according to the defined structure fields [305]

Each error object within the errors array MUST NOT be empty and MUST contain at least one of the following attributes:

field                        description
idA unique identifier for this particular occurrence of the problem.
codeAn application-specific error code, expressed as a string value. The format and type of code representation (such as, numeric values or hex values) MUST be harmonized across all error codes within an application.
The code focuses on programs and doesn’t have to be human-readable.
statusNumeric HTTP status code for the specific error.
titleDeveloper friendly, human-readable description or summary that SHOULD NOT change from occurrence to occurrence of the problem.
In case of using a custom HTTP status codes in the status field of the error object, the title MUST provide a concise description of the HTTP error code (for example: status: "599", title: "Network Connection Timeout").
detailDeveloper friendly, human-readable, detailed description specific to the occurrence of the problem.
linksA links object is a resource object in its own. links point to further information for the reported error to support the developer to fix the problem.
correlationIdA unique string identifier, e.g. a UUID, representing a flow through the system. It can be used for tracing and debugging, see Best Practices.

An API MAY provide additional attributes.

Usage of the property code in error object

Be aware of the possibility to misuse the code for hack attacks. Consider the rule to Not Expose Stack Traces of Your Error" for not exposing the call stack of the application, the same is valid for the application specific code. Values like Access Violation provides more details about the root cause.

Extending the property code to track error origin

In a distributed system, such as, microservices architecture there are transitive calls happening. To state the origin of the error, the calling service MAY report the received error to its caller too. To differ the origin of the errors in the list, the code can be prefixed with an abbreviation of the service, like "sgp:0x80003033" to report, that the error 0x80003033 was initially reported by service sgp (Siemens GPS Position service). This common practice improves the inspectability and understandability of errors. But the prefix SHOULD NOT expose too much details for the application system architecture.

The links resource object MAY contain the following members:

  • about: MUST provide a URI that redirects to further details about this particular occurrence of the error. When opened, this URI SHOULD return a human-readable description of the error for the developer to investigate.
  • type: MUST provide a URI that identifies the type of error that this particular error belongs to. The URI points to a human-readable explanation of the error type for the developer to investigate.

Here is an example of a simple error response.

{
  "errors": [
    {
      "code":   "0x80003033"
    }
  ]
}

In the above example HTTP header already includes status and title, so there is no need of repetition.

In case the application wants to point in the error object to the primary source of the problem, the property source MAY be used. The source object SHOULD include one of the following members or be omitted:

  • pointer: a RFC6901 JSON Pointer to the value in the request document that caused the error (for example, "/data" for a primary data object, or "/data/attributes/title" for a specific attribute). This MUST point to a value in the request document that exists; if it doesn’t, the API client SHOULD simply ignore the pointer.
  • parameter: a string that indicates which URI query parameter caused the error.
  • header: a string that indicates the name of the header property which caused the error.

Here is an example of a detailed error response.

{
  "errors": [
    {
      "id": "eec33bf0-6bcc-4813-ae7e-0a70e8e53c3b",
      "code": "0x00000001",
      "status": 415,
      "title": "Unsupported Media Type",
      "detail": "The requested content type is not supported",
      "source": {
        "header": "content-type"
      },
      "links": {
        "about": "https://applicationx.siemens.net/validation-error/overview/#content-type",
      }
    },
    {
      "id": "e043cedd-600c-468c-8563-d4e591e3ba89",
      "code": "0x30005553",
      "detail": "the device name must not include any other characters than a-z, A-Z, 0-9, - and _",
      "title": "Unprocessable Content",
      "source": {
        "pointer": "/device/attributes/deviceName"
      },
      "links": {
        "about": "https://applicationx.siemens.net/validation-error/overview/#devices",
      }
    },
    {
      "id": "fd5864bd-3233-4f8d-9da2-734910be43bb",
      "code":   "0x80003033",
      "status": 410,
      "detail": "The device with name is already gone"
    }
  ]
}

The values of the code field SHOULD be unique [305.1]

Having a unique error code per error class eases the error handling of API clients.

All error codes SHOULD be documented [305.2]

All possible error codes SHOULD be documented with their corresponding descriptions in the API documentation. This allows API clients to decide which errors need to be translated or handled in another way.

The values of the title and detail fields SHOULD be in English [305.3]

Generally, error messages SHOULD be provided in English only for several reasons. One reason is that these errors mostly address developers.