The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content

Industrial Edge is an open, ready-to-use edge computing platform, with edge devices, edge applications (apps) and connectivity through an integrated app and device management infrastructure.

Industrial Edge

What is Industrial Edge?

Siemens Industrial Edge (IE) is an open, ready-to-use edge computing platform, with edge devices, edge applications (apps) and connectivity through an integrated app and device management infrastructure. It allows you to easily connect, manage and operate globally distributed edge installations, with your own or the diverse apps available through the Industrial Edge Marketplace.

Industrial Edge Ecosystem

The Industrial Edge Ecosystem is for your implementation and usage, if you are an industrial producer or machine producer. You can connect, create, deploy and scale your industrial use case using the Industrial Edge platform in combination with apps, devices and solutions from the Industrial Edge Ecosystem. You may also develop your own apps and deploy them via the Industrial Edge Management.

Industrial Edge Devices

A wide range of Industrial Edge devices makes it easy to deploy edge computing in your production environment: You can use SIMATIC controllers and HMIs with integrated edge functionality, use IPCs and virtualized systems, and obtain certified edge devices from our Industrial Edge Ecosystem partners.

Industrial Edge Device website

Industrial Edge Apps

Customers can develop and deploy their own apps, or buy ready-made apps and existing connectivity from the catalogue on the Industrial Edge Marketplace. These apps from Siemens and Ecosystem partners work for more than 90 % of automation systems.

Find all available Industrial Edge apps here: Industrial Edge Marketplace

Developer Resources

Learn how to use Industrial Edge and start developing your own apps.

LinkDescription
Developer DocumentationDeveloper Documentation.
Developer GuideIntroduction to industrial Edge Development
Industrial Edge API ReferenceIndustrial Edge APIs and References
Industrial Edge Playground RegistrationRequest Access for the Industrial Edge Playground
GitHubIndustrial Edge on GitHub
About DockerDocker is the technology to run, deploy and create Industrial Edge apps using containers.
Industrial Edge Release NotesIndustrial Edge Release Notes
SITRAIN Digital Industry AcademyCourse: App Development Workflow for Industrial Edge (24 Hours)

Device Builder Resources

Device Builders can build own device offerings based on Industrial Edge. This includes the development of the device, the integration of the Industrial Edge packages, system tests, support and maintenance of the device offered within the Ecosystem. As a Device Builder, they are partner of the Industrial Edge Ecosystem and can provide added value by selling their Industrial Edge Devices to all participants.

LinkDescription
Device Builder Quick StartDevice Builder Quick Start.
Device Builder GuideDevice Builder Guide

Device Builder- IE Device Kit API

The IE Device Kit API provides the abstraction layer that decouples the Industrial Edge Runtime from the underlying Linux systems. This allows to adapt the runtime and its behavior to serve for the specific needs of different Industrial Edge products.

The IE Device Kit API is based on gRPC which provides a modern intermediate process communication style for building distributed applications and microservices. The Industrial Edge platform provides and maintains the protobuf specification files for the APIs contained in the IE Device Kit. These protobuf specifications can be used to create stub implementations for both client and server in various programming languages. The Industrial Edge Runtime ships with a client side implementation of these APIs and expects the host system to provide a server side implementation.

LinkDescription
IE Device Kit System ServiceSystem Service is a gRPC & Go based system resource tracker and system controller.
IE Device Kit Onboard ServiceOnboard Service is a gRPC & Go based Edge Core activator. This service communicates with all other services and provides the necessary configurations for the Edge Device to successfully onboard to Industrial Edge Management system.
IE Device Kit Ntp ServiceNTP Service is a gRPC & Go based NTP configurator microservice for Edge Devices.
IE Device Kit Network ServiceNetwork Service is a gRPC & Go based network configuration microservice. The network settings of the Edge Devices are configured through this service.

Mendix on Edge

Mendix on Edge integrates the software development capabilities of Mendix to the Industrial Edge allowing IT and OT people to develop applications with low-code for the shopfloor. With Mendix on Edge we enhance the Industrial Edge offering for every customer developing own applications.

Mendix on Edge

Providing an integrated low-code development tool with Mendix on Edge aims to support development of own apps (Make vs. Buy scenario) even for users without extensive IT knowledge.

Low-code on the shopfloor, speeds up app development, enables local deployment of Mendix apps for decentralized and real time data processing, secure OT operation, secure connectivity and transmission across OT and IT systems.

Which components are needed to build Mendix apps for Industrial Edge?¶ In order to push and use Mendix applications in Industrial Edge you need two components:

Download and install the Industrial Edge Plugin for Mendix Studio Pro for free from the Mendix Marketplace. Once installed, follow the wizard to publish your applications to your IE Hub or IE Management system.

For each IE Device that runs Mendix applications you need to obtain a Mendix Device License from the Marketplace. The license entitles you to develop, install and run an unlimited number of Mendix applications on one single Industrial Edge Device with a maximum of 10 named users per app instance and a maximum main memory of 4, 8, 16, 32 or 64 GB (RAM), depending on the selected subscription.

Learn more about Mendix on Edge

LinkDescription
Mendix on EdgeDevelop Industrial Edge Apps using the Mendix low-code development platform
Mendix AcademyCourse: Build your Industrial Edge App with Mendix (4 hours)
Mendix on Edge DocumentationMendix on Edge Documentation