The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

MindConnect-NodeJS - Agent Development - Retrying the operations

Making sure that the data arrives also with an unreliable internet connection

You can wrap all asynchronous object calls into the retry function which will automatically retry the operation for n times before throwing an exception.

import {
    MindConnectAgent,
    Insights HubStandardEvent,
    retry,
    TimeStampedDataPoint,
} from "@mindconnect/mindconnect-nodejs";

// if you want to be more resillient you can wrap every async method
// in the retry function which will try to retry several 
// times before throwing an exception

// onboarding over flaky connection
await retry(5, () => agent.OnBoard());

// bulk upload with 5 retries
const bulk: TimeStampedDataPoint[] = [
    {
        timestamp: "2018-08-23T18:38:02.135Z",
        values: [
            { dataPointId: "DP-Temperature", qualityCode: "0", value: "10" },
            { dataPointId: "DP-Pressure", qualityCode: "0", value: "10" },
        ],
    },
    {
        timestamp: "2018-08-23T19:38:02.135Z",
        values: [
            { dataPointId: "DP-Temperature", qualityCode: "0", value: "10" },
            { dataPointId: "DP-Pressure", qualityCode: "0", value: "10" },
        ],
    },
];

await retry(5, () => agent.BulkPostData(bulk));

Uploading large files with multipart upload

For the large files upload you would typically want to retry only the upload operations of the chunks and not the whole multipart upload once an error occurs. Therefore the UploadFile method offers the possibility to retry only the chunked upload:

// the upload-file can be a multipart operation and therefore can 
// be configured to retry the upload of the chunks instead 
// of the upload of the whole file.
// if you don't specify the type, 
// the mimetype is automatically determined by the library

await agent.UploadFile(agent.ClientId(), 
  "custom/mindsphere/path/package.json", 
  "package.json", {
    retry: RETRYTIMES,
    description: "File uploaded with MindConnect-NodeJS Library",
    chunk: true, // the chunk parameter activates multipart upload
});