The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

Mindconnect-NodeJS - Agent Development - Starter Projects

Introduction

The easiest way to start the development is to use the CLI to generate the starter projects

Prerequisites

You will need the installed CLI.

Step 1 - Create the project with help of the CLI

Example

Use the CLI to setup a starter project called my-agent:

mdsp createts --dir my-agent

This will provide following output:

Starter project in my-agent has been created.
Please run npm install in my-agent directory to install dependecies.
# after this we will install the required dependencies

cd my-agent
npm install

After this create the agentconfig.json with help of the CLI:

mdsp create-agent --passkey{your passkey} --config agentconfig.json

This will produce following output

Configure your agent at:

        https://{yourtenant}-assetmanager.eu1.mindsphere.io/entity/{agentid}/plugin/uipluginassetmanagermclib

Step 2 - Create the assets in Insights Hub

Create aspect types, asset type and asset in InsightsHub. Remember your asset id.

Step 3 - Configure the agent

You can use the new automatic creation of DataSourceConfiguration and DataSourceMappings to configure your agent.

import {
  DataPointValue,
  MindConnectAgent,
  MindSphereStandardEvent,
  retry,
  TimeStampedDataPoint,
} from "@mindconnect/mindconnect-nodejs";

(async function () {
  const sleep = (ms: any) => new Promise((resolve) => setTimeout(resolve, ms));
  const configuration = require("../../agentconfig.json");
  const agent = new MindConnectAgent(configuration);
  const log = (text: any) => {
    console.log(`[${new Date().toISOString()}] ${text.toString()}`);
  };
  const RETRYTIMES = 5; // retry the operation before giving up and throwing exception

  // onboarding the agent
  // Check in the local agent state storage if agent is onboarded.

if (!agent.IsOnBoarded()) {
    // wrapping the call in the retry function makes the agent a bit more resillient
    // if you don't want to retry the operations you can always just call await agent.OnBoard(); instead.
    await retry(RETRYTIMES, () => agent.OnBoard());
    log("Agent onboarded");
  }

  // you can use agent.Sdk().GetAssetManagementClient() to get the asset id and asset type from Insights Hub.
  const targetAssetId = "1234567....";
  const targetAssetType = `${agent.GetTenant()}.Engine`;

  // create data sourceconfiguration and mappings

  // this generates a data source configuration from an asset type
  const config = await agent.GenerateDataSourceConfiguration(targetAssetType);

  // create/overwrite the data source configuration
  await agent.PutDataSourceConfiguration(config);

  // create mappings for asset id
  const mappings = await agent.GenerateMappings(targetAssetId);
  // store mappings in InsightsHub
  await agent.PutDataMappings(mappings);

  // instead of creating the data source configuration and mappings separately
  // you can also just use the method below which takes care of everything
  // this is only used for 1:1 asset -> agent mappings
  // the method above can also map the data source configuration to multiple assets
  // just call GenerateMappings with different asset ids

  await agent.ConfigureAgentForAssetId(targetAssetId);

  // Check in the local agent state storage if agent has data source configuration.
  if (!agent.HasDataSourceConfiguration()) {
    await retry(RETRYTIMES, () => agent.GetDataSourceConfiguration());
    log("Configuration aquired");
  }

  for (let index = 0; index < 5; index++) {
    try {
      log(`Iteration : ${index}`);

      // if you have configred the data points in the Insights Hub UI you will have to use the long integer values instead of descriptive dataPointIds.

      const values: DataPointValue[] = [
        {
          dataPointId: "DP-Temperature",
          qualityCode: "0",
          value: (Math.sin(index) * (20 + (index % 2)) + 25).toString(),
        },
        {
          dataPointId: "DP-Pressure",
          qualityCode: "0",
          value: (Math.cos(index) * (20 + (index % 25)) + 25).toString(),
        },
        {
          dataPointId: "DP-Humidity",
          qualityCode: "0",
          value: ((index + 30) % 100).toString(),
        },
        {
          dataPointId: "DP-Acceleration",
          qualityCode: "0",
          value: (1000.0 + index).toString(),
        },
        {
          dataPointId: "DP-Frequency",
          qualityCode: "0",
          value: (60.0 + index * 0.1).toString(),
        },
        {
          dataPointId: "DP-Displacement",
          qualityCode: "0",
          value: (index % 10).toString(),
        },
        {
          dataPointId: "DP-Velocity",
          qualityCode: "0",
          value: (50.0 + index).toString(),
        },
      ];

      // same like above, you can also just call  await agent.PostData(values) if you don't want to retry the operation
      // this is how to send the data with specific timestamp
      // await agent.PostData(values, new Date(Date.now() - 86400 * 1000));

      await retry(RETRYTIMES, () => agent.PostData(values));
      log("Data posted");
      await sleep(1000);

      const event: MindSphereStandardEvent = {
        entityId: agent.ClientId(), // use assetid if you want to send event somewhere else :)
        sourceType: "Event",
        sourceId: "application",
        source: "Meowz",
        severity: 20, // 0-99 : 20:error, 30:warning, 40: information
        timestamp: new Date().toISOString(),
        description: "Test",
      };

      // send event with current timestamp; you can also just call agent.PostEvent(event) if you don't want to retry the operation
      await retry(RETRYTIMES, () => agent.PostEvent(event));
      log("event posted");
      await sleep(1000);

      // upload file
      // the upload-file can be a multipart operation and therefore can be configured to
      // retry the upload of the chunks instead the upload of the whole file.
      // if you don't specify the type , the mimetype is automatically determined by the library
      await agent.UploadFile(
        agent.ClientId(),
        "custom/mindsphere/path/package.json",
        "package.json",
        {
          retry: RETRYTIMES,
          description: "File uploaded with MindConnect-NodeJS Library",
          chunk: true, // the chunk parameter activates multipart upload
        }
      );

      log("file uploaded");
      await sleep(1000);

      const yesterday = new Date();
      yesterday.setDate(yesterday.getDate() - 1);
      const bulk: TimeStampedDataPoint[] = [
        {
          timestamp: yesterday.toISOString(),
          values: [
            { dataPointId: "DP-Temperature", qualityCode: "0", value: "10" },
            { dataPointId: "DP-Pressure", qualityCode: "0", value: "10" },
          ],
        },
        {
          timestamp: new Date().toISOString(),
          values: [
            { dataPointId: "DP-Temperature", qualityCode: "0", value: "10" },
            { dataPointId: "DP-Pressure", qualityCode: "0", value: "10" },
          ],
        },
      ];

      await retry(RETRYTIMES, () => agent.BulkPostData(bulk));
      log("bulk data uploaded");
      await sleep(1000);
    } catch (err) {
      // add proper error handling (e.g. store data somewhere, retry later etc. )
      console.error(err);
    }
  }
})();

Start the agent

npm start

This should produce the output like this:

> mc-agent-ts@1.0.0 start 
> tsc && node index.js

[2019-05-17T15:41:11.375Z] Iteration : 0
[2019-05-17T15:41:13.495Z] Agent onboarded
[2019-05-17T15:41:14.398Z] Configuration aquired
[2019-05-17T15:41:14.958Z] Data posted
[2019-05-17T15:41:16.409Z] event posted
[2019-05-17T15:41:18.285Z] bulk data uploaded
[2019-05-17T15:41:19.288Z] Iteration : 1
[2019-05-17T15:41:19.716Z] Data posted
[2019-05-17T15:41:21.325Z] event posted
[2019-05-17T15:41:23.445Z] bulk data uploaded
[2019-05-17T15:41:24.447Z] Iteration : 2
[2019-05-17T15:41:24.886Z] Data posted
[2019-05-17T15:41:26.289Z] event posted
[2019-05-17T15:41:30.744Z] bulk data uploaded