The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp agent-status Command

Syntax:

mdsp agent-status

Help:

mdsp agent-status --help

Alternative form:

mc agent-status

(The CLI was using mc as default command name in older versions)

Description

displays the agent status and agent onboarding status *

Usage

Parameter list:

Usage: mdsp agent-status|as [options]

displays the agent status and agent onboarding status *

Options:
 -c, --config config file with agent configuration
 -a, --agentid agentid
 -k, --passkey passkey
 -r, --cert [privatekey] required for agents with RSA_3072 profile. create with: openssl genrsa -out private.key 3072
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp agent-status command:

 Examples:

 mdsp agent-status uses default agentconfig.json
 mdsp agent-status --config agent.json uses specified configuration file
 mdsp agent-status --cert private.key uses specified key for RSA_3072 profile
 mdsp agent-status --passkey mypasskey displays also the online agent information
 mdsp agent-status --passkey mypasskey --verbose displays additionally the mappings and configuration

See Insights Hub API documentation for more information about Insights Hub APIs.