The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp aspects Command

Syntax:

mdsp aspects

Help:

mdsp aspects --help

Alternative form:

mc aspects

(The CLI was using mc as default command name in older versions)

Description

list, create or delete aspects *

Usage

Parameter list:

Usage: mdsp aspects|asp [options]

list, create or delete aspects *

Options:
 -m, --mode [list|create|delete|convert|template|info] list | create | delete | convert | template | info (default: "list")
 -f, --file .mdsp.json file with aspect type definition
 -s, --schema JSON Schema
 -n, --aspect the aspect type name
 -p, --prefixflattened prefix variable names with previous name when flattening schema
 -t, --targetonly consider only variables which have target equal to aspect in schema
 -u, --untargeted consider only variables which don't have target in schema
 -l, --length default string length (default: "255")
 -b, --biglength default bigstring length (default: "5000")
 -i, --idonly list only ids
 -c, --includeshared include shared aspect types
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp aspects command:

 Examples:

 mdsp aspects --mode list list all aspect types
 mdsp aspects --mode list --aspect Environment list all aspect types which are named Environment
 mdsp aspects --mode template --aspect Environment 
 create a template file (Enironment.aspect.mdsp.json) for aspect Environment
 mdsp aspects --mode create --file Environment.aspects.mdsp.json 
 create aspect type Environment in Insights Hub
 mdsp aspects --mode convert --schema Environment.schema.json --aspect Environment 
 create a template file for aspect type Environment from JSON schema
 mdsp aspects --mode convert --schema Environment.schema.json --aspect Environment --prefixflattened 
 prefixes the variable names with parent object names (e.g. Environment_Temperature)
 mdsp aspects --mode convert --schema Environment.schema.json --aspect Environment --targetonly 
 select only variables from json schema with target property equal to assettype

See Insights Hub API documentation for more information about Insights Hub APIs.