The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp assets Command

Syntax:

mdsp assets

Help:

mdsp assets --help

Alternative form:

mc assets

(The CLI was using mc as default command name in older versions)

Description

list, create or delete assets *

Usage

Parameter list:

Usage: mdsp assets|ast [options]

list, create or delete assets *

Options:
 -m, --mode [list|create|delete|template|tree] mode [list | create | delete | template | tree] (default: "list")
 -f, --file .mdsp.json file with asset definition
 -n, --assetname assetname
 -p, --parentid parentid
 -e, --externalid externalid
 -i, --assetid Insights Hub asset id
 -t, --typeid typeid
 -d, --desc description (default: "created with Insights Hub CLI")
 -w, --twintype digital twin type [performance|simulation]
 -c, --includeshared include shared aspect types
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp assets command:

 Examples:

 mdsp assets --mode create --typeid core.basicarea --assetname MyArea creates an asset in Insights Hub of type basicarea
 mdsp assets --mode create --file MyPump.asset.mdsp.json creates an asset from specified file template
 mdsp assets --mode list lists all assets in Insights Hub
 mdsp assets --mode list --typeid mclib lists all assets in Insights Hub of type core.mclib
 mdsp assets --mode delete --assetid 1234567..ef deletes asset with specified id from Insights Hub
 mdsp assets --mode template --typeid .Pump --assetname MyPump 
 creates a file template MyPump.asset.mdsp.json which can be use in create command

See Insights Hub API documentation for more information about Insights Hub APIs.