The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp cases Command

Syntax:

mdsp cases

Help:

mdsp cases --help

Alternative form:

mc cases

(The CLI was using mc as default command name in older versions)

Description

list, create or delete cases *

Usage

Parameter list:

Usage: mdsp cases|cs [options]

list, create or delete cases *

Options:
  -m, --mode [list|create|update|delete|template|info]  list | create | update | delete | template | info (default:
                                                        "list")
  -f, --file                                      .mdsp.json file with case definition (default: "case.mdsp.json")
  -n, --case                                      the case name
  -i, --handle                                  the case handle
  -o, --overwrite                                       overwrite template file if it already exists
  -k, --passkey                                passkey
  -y, --retry                                   retry attempts before giving up (default: "3")
  -v, --verbose                                         verbose output
  -h, --help                                            display help for command

Examples

Here are some examples of how to use the mdsp cases command:

  Examples:

    mdsp cases --mode list                                  list all cases
    mdsp cases --mode template --case                       create a template file for 
    mdsp cases --mode create --file                         create case 
    mdsp cases --mode update --file  --handle <handle>      update case 
    mdsp cases --mode info --handle  <handle>               case info for specified handle
    mdsp cases --mode delete --handle <handle>              delete case with specified handle

See MindSphere API documentation for more information about MindSphere APIs.