The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp configure-agent Command

Syntax:

mdsp configure-agent

Help:

mdsp configure-agent --help

Alternative form:

mc configure-agent

(The CLI was using mc as default command name in older versions)

Description

create data source configuration and mappings (optional: passkey) *

Usage

Parameter list:

Usage: mdsp configure-agent|co [options]

create data source configuration and mappings (optional: passkey) *

Options:
 -c, --config config file with agent configuration
 -m, --mode [mode] command mode [config|map|print|delete|test|func|template] (default: "config")
 -a, --agentid agentid
 -i, --assetid target assetid for mapping
 -t, --typeid asset type for configuration
 -l, --language [js|python|json] target language for conversion function (default: "js")
 -s, --timespan timespan between generated timestamps (in ms) (default: "1000")
 -c, --count Number of generated records (default: "10")
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp configure-agent command:

 Examples:

 mdsp configure-agent --config agent.json -assetid 1234567...89 configures agent for specified assetid
 mdsp configure-agent --config agent.json --mode print prints data source configuration and mappings
 mdsp configure-agent --agentid 12345..ef --typeid .Engine creates the data source configuration
 mdsp configure-agent --mode map --agentid 12345..ef --assetid 1234567 creates the mappings for assetid
 mdsp configure-agent --mode delete --agentid 12345..ef deletes the mappings for agentid
 mdsp configure-agent --config agent.json --mode test sends test data to Insights Hub
 mdsp configure-agent --mode template \
 --typeid castidev.Pump --language python create mapping template and function in python

See Insights Hub API documentation for more information about Insights Hub APIs.