The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp create-event Command

Syntax:

mdsp create-event

Help:

mdsp create-event --help

Alternative form:

mc create-event

(The CLI was using mc as default command name in older versions)

Description

create an event in the Insights Hub (optional: passkey) *

Usage

Parameter list:

Usage: mdsp create-event|ce [options]

create an event in the Insights Hub (optional: passkey) *

Options:
 -c, --config config file with agent configuration
 -r, --cert [privatekey] required for agents with RSA_3072 profile. create with: openssl genrsa -out private.key 3072
 -i, --assetid Insights Hub asset id (default: send event to the agent)
 -y, --sourceType Source Type (default: "MindConnect-Agent")
 -S, --sourceId Source Id (default: "Monikas-Air-2.fritz.box")
 -O, --source Source (default: "MindConnect-NodeJs CLI")
 -V, --severity Severity (20:Error, 30:Warning , 40:information) (default: "20")
 -d, --desc Event description (default: "CLI created event")
 -t, --timestamp Timestamp (default: "2022-11-06T01:51:16.184Z")
 -y, --retry retry attempts before giving up (default: "3")
 -p, --passkey passkey (optional, event creation uses service credentials *)
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp create-event command:

 Examples:

 mdsp create-event create error event with default values and current timestamp
 mdsp ce --desc Warning! --severity 30 create warning with description warning
 mdsp ce --desc "custom event" --i 123....4 create error event for asset with id 123....4

See Insights Hub API documentation for more information about Insights Hub APIs.