The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp download-file Command

Syntax:

mdsp download-file

Help:

mdsp download-file --help

Alternative form:

mc download-file

(The CLI was using mc as default command name in older versions)

Description

download the file from Insights Hub file service *

Usage

Parameter list:

Usage: mdsp download-file|df [options]

download the file from Insights Hub file service *

Options:
 -f, --file file to download from the file service
 -h, --filepath [filepath] file path in the Insights Hub (default: "")
 -i, --assetid Insights Hub asset id
 -p, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 --help display help for command

Examples

Here are some examples of how to use the mdsp download-file command:

 Examples:

 mdsp download-file -f CHANGELOG.md --assetid 5..f download file CHANGELOG.md from specified asset
 mdsp download-file --file CHANGELOG.md --assetid 5...f --filepath upload download file upload/CHANGELOG.md from specified asset
 mdsp download-file --file upload/CHANGELOG.md --assetid 5...f download file upload/CHANGELOG.md from specified asset

See Insights Hub API documentation for more information about Insights Hub APIs.