Skip to content
Siemens Developer Portal

mdsp event-analytics Command

Syntax:

mdsp event-analytics

Help:

mdsp event-analytics --help

Alternative form:

mc event-analytics

(The CLI was using mc as default command name in older versions)

Description

analyze Insights Hub events @

Usage

Parameter list:

Usage: mdsp event-analytics|ea [options]

analyze Insights Hub events @

Options:
 -m, --mode [count|filter|duplicate|top] mode see @ Additional Documentation (default: "top")
 -f, --file events file
 -o, --output result mode.ea.mdsp.json
 -t, --type [timeseries|event] event analytics can be used on both timeseries (with string properties as event names) and event
 formats (default: "event")
 -p, --property property name used for grouping and counting (default: "description")
 -l, --filterlist filter events (default: "[]")
 -x, --top number of events (for top mode) (default: "10")
 -s, --split split interval (for count, duplicate) (default: "5000")
 -y, --retry retry attempts before giving up (default: "3")
 -p, --passkey passkey
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp event-analytics command:

 Examples:

 mdsp event-analytics --mode top --file events.json --property description find the top 10 events in events.json
 mdsp event-analytics --mode duplicate --file events.json --property description --split 5000 remove all duplicate events

 Additional Documentation:

 https://developer.mindsphere.io/apis/analytics-eventanalytics/api-eventanalytics-overview.html
 https://developer.mindsphere.io/apis/analytics-eventanalytics/api-eventanalytics-samples.html

See Insights Hub API documentation for more information about Insights Hub APIs.

Community

Connect and Collaborate with Industrial Professionals and Join the Community!

Click to load comments