The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp event-types Command

Syntax:

mdsp event-types

Help:

mdsp event-types --help

Alternative form:

mc event-types

(The CLI was using mc as default command name in older versions)

Description

list, create or delete event types *

Usage

Parameter list:

Usage: mdsp event-types|et [options]

list, create or delete event types *

Options:
 -m, --mode [list|create|delete|template|info] list | create | delete | template | info (default: "list")
 -f, --file .mdsp.json file with event type definition
 -i, --idonly list only ids
 -s, --schema JSON Schema
 -n, --eventtype the event type name
 -c, --includeshared include shared event types
 -g, --includeglobal include global event types
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp event-types command:

 Examples:

 mdsp event-types --mode list list all event types
 mdsp event-types --mode list --eventtype PumpEvent list all event types which are named PumpEvent
 mdsp event-types --mode template --eventtype PumpEvent 
 create a template file (PumpEvent.eventtype.mdsp.json) for event type PumpEvent
 mdsp event-types --mode create --file PumpEvent.eventtype.mdsp.json 
 create event type PumpEvent in Insights Hub

See Insights Hub API documentation for more information about Insights Hub APIs.