The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp markdown-help Command

Syntax:

mdsp markdown-help

Help:

mdsp markdown-help --help

Alternative form:

mc markdown-help

(The CLI was using mc as default command name in older versions)

Description

generates folder with markdown help commands for the CLI*

Usage

Parameter list:

Usage: mdsp markdown-help|mdhelp [options]

generates folder with markdown help commands for the CLI*

Options:
 -d, --dir folder folder (default: "markdown-help")
 -o, --overwrite overwrite files if they already exist
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp markdown-help command:

 Examples:

 mdsp mdhelp

See Insights Hub API documentation for more information about Insights Hub APIs.