The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp oe-devices Command

Syntax:

mdsp oe-devices

Help:

mdsp oe-devices --help

Alternative form:

mc oe-devices

(The CLI was using mc as default command name in older versions)

Description

list, create or delete (open edge) devices *

Usage

Parameter list:

Usage: mdsp oe-devices|oed [options]

list, create or delete (open edge) devices *

Options:
 -m, --mode [list|create|delete|template|info] list | create | delete | template | info (default: "list")
 -f, --file .mdsp.json file with device definition
 -n, --devicename device name
 -a, --assetid the id of the asset linked to the device
 -t, --typeid the device type id
 -d, --desc description (default: "created with Insights Hub CLI")
 -s, --serialnumber the id of the asset linked to the device
 -i, --id the device id
 -o, --overwrite overwrite template file if it already exists
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp oe-devices command:

 Examples:

 mdsp oe-devices --mode list --assetid list all devices linked to the asset
 mdsp oe-devices --mode info --id get device details
 mdsp oe-devices --mode template create a template file for a new device
 mdsp oe-devices --mode delete --id delete the device with the specified id
 mdsp oe-devices --mode create --file openedge.device.mdsp.json 
 create new device using the file openedge.device.mdsp.json

See Insights Hub API documentation for more information about Insights Hub APIs.