The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp sdi-file-upload Command

Syntax:

mdsp sdi-file-upload

Help:

mdsp sdi-file-upload --help

Alternative form:

mc sdi-file-upload

(The CLI was using mc as default command name in older versions)

Description

upload file to SDI *

Usage

Parameter list:

Usage: mdsp sdi-file-upload|sdu [options]

upload file to SDI *

Options:
 -f, --file file to upload to SDI
 -h, --filepath file path in SDI
 -m, --mime [mime-type] mime type of the file (default: automatic recognition)
 -y, --retry retry attempts before giving up (default: "3")
 -k, --passkey passkey
 -v, --verbose verbose output
 --help display help for command

Examples

Here are some examples of how to use the mdsp sdi-file-upload command:

 Examples:

 mdsp sdi-file-upload --file upload file to SDI

 Restriction:

 This works only for SDI only tenants (without Integrated Data Lake)
 If you are Insights Hub Integrated Data Lake Customer use mdsp data-lake --mode upload command instead. 

See Insights Hub API documentation for more information about Insights Hub APIs.