The chat responses are generated using Generative AI technology for intuitive search and may not be entirely accurate. They are not intended as professional advice. For full details, including our use rights, privacy practices and potential export control restrictions, please refer to our Generative AI Service Privacy Information. As this is a test version, please let us know if something irritating comes up. Like you get recommended a chocolate fudge ice cream instead of an energy managing application. If that occurs, please use the feedback button in our contact form!
Skip to content
Industrial IoT Open Source Tools and Libraries Share llms optimized content

Demo applications, libraries and SDKs as well as useful connectivity tools which are maintained and released as open source software.

mdsp sdi-ontologies Command

Syntax:

mdsp sdi-ontologies

Help:

mdsp sdi-ontologies --help

Alternative form:

mc sdi-ontologies

(The CLI was using mc as default command name in older versions)

Description

manage ontologies for SDI *

Usage

Parameter list:

Usage: mdsp sdi-ontologies|sdo [options]

manage ontologies for SDI *

Options:
 -m, --mode [list|infer|update|template|info|delete] list | infer | update | template | info | delete (default: "list")
 -d, --ontology ontology file with definition for --mode infer or update command
 -i, --ontologyid the ontology id for --mode info, update or delete command
 -o, --overwrite overwrite template file if it already exists
 -k, --passkey passkey
 -y, --retry retry attempts before giving up (default: "3")
 -v, --verbose verbose output
 -h, --help display help for command

Examples

Here are some examples of how to use the mdsp sdi-ontologies command:

 Examples:

 mdsp sdi-ontologies --mode list list all sdi ontologies
 mdsp sdi-ontologies --mode template create template file
 mdsp sdi-ontologies --mode infer --ontology infer sdi ontology
 mdsp sdi-ontologies --mode info --ontologyid get sdi ontology info
 mdsp sdi-ontologies --mode delete --ontologyid delete sdi ontology

See Insights Hub API documentation for more information about Insights Hub APIs.